<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K314 DataFlash emulates EEPROM</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-DataFlash-emulates-EEPROM/m-p/1471571#M15873</link>
    <description>&lt;P&gt;On this device there EEPROM is emulated by SW in the data flash. For understanding the principle I could recommend following appnote (although written for different platform, the principle is the same): &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4868.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4868.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Driver and example project you may find in S32DS, it is called Fee_Example_S32K3xx.&lt;/P&gt;
&lt;P&gt;In the installation directory, you may also find user manual for Flash EEPROM emulation driver:&lt;BR /&gt;c:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2021_10\SW32K3_RTD_4_4_1_0_0_D2110\Fee_TS_T40D34M10I0R0\doc\&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jun 2022 14:22:46 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2022-06-09T14:22:46Z</dc:date>
    <item>
      <title>S32K314 DataFlash emulates EEPROM</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-DataFlash-emulates-EEPROM/m-p/1469864#M15821</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;According to the description in Section 20.5.5 of S32K3XXRM.pdf, S32K314 supports DataFlash emulated EEPROM, but this part is more general.&lt;BR /&gt;Where can I get the detailed information of EEPROM emulation and the sample project for S32K314?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 09:01:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-DataFlash-emulates-EEPROM/m-p/1469864#M15821</guid>
      <dc:creator>Danny_Wu</dc:creator>
      <dc:date>2022-06-07T09:01:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 DataFlash emulates EEPROM</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-DataFlash-emulates-EEPROM/m-p/1471571#M15873</link>
      <description>&lt;P&gt;On this device there EEPROM is emulated by SW in the data flash. For understanding the principle I could recommend following appnote (although written for different platform, the principle is the same): &lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4868.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4868.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Driver and example project you may find in S32DS, it is called Fee_Example_S32K3xx.&lt;/P&gt;
&lt;P&gt;In the installation directory, you may also find user manual for Flash EEPROM emulation driver:&lt;BR /&gt;c:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2021_10\SW32K3_RTD_4_4_1_0_0_D2110\Fee_TS_T40D34M10I0R0\doc\&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 14:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-DataFlash-emulates-EEPROM/m-p/1471571#M15873</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-06-09T14:22:46Z</dc:date>
    </item>
  </channel>
</rss>