<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 s32k144 Lin packet timeout error</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-Lin-packet-timeout-error/m-p/1471447#M15870</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;Because I want to use S32K144 to send Lin messages, I download Lin host routines to the development board, and use PLIN to monitor the messages. &lt;/SPAN&gt;&lt;SPAN class=""&gt;According to the routines, I should press SW3 to wake up Lin, and then press SW2 to send messages ,but in fact, press SW3 to monitor the messages a&lt;SPAN&gt;nd displays a timeout error&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;, sw2 does not respond, and I only change the baud rate and checksum type to monitor the packets. &lt;/SPAN&gt;&lt;SPAN class=""&gt;I really do not understand, hope to get a solution. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Routines used: lin_master_baremetal_s32k144; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Changes: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Baud rate: 9600 ——&amp;gt;19200; &lt;/SPAN&gt;&lt;SPAN class=""&gt;Checksum type: classic——&amp;gt;Enhanced&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jun 2022 11:41:16 GMT</pubDate>
    <dc:creator>kalajiao</dc:creator>
    <dc:date>2022-06-09T11:41:16Z</dc:date>
    <item>
      <title>s32k144 Lin packet timeout error</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-Lin-packet-timeout-error/m-p/1471447#M15870</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Because I want to use S32K144 to send Lin messages, I download Lin host routines to the development board, and use PLIN to monitor the messages. &lt;/SPAN&gt;&lt;SPAN class=""&gt;According to the routines, I should press SW3 to wake up Lin, and then press SW2 to send messages ,but in fact, press SW3 to monitor the messages a&lt;SPAN&gt;nd displays a timeout error&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;, sw2 does not respond, and I only change the baud rate and checksum type to monitor the packets. &lt;/SPAN&gt;&lt;SPAN class=""&gt;I really do not understand, hope to get a solution. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Routines used: lin_master_baremetal_s32k144; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Changes: &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Baud rate: 9600 ——&amp;gt;19200; &lt;/SPAN&gt;&lt;SPAN class=""&gt;Checksum type: classic——&amp;gt;Enhanced&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 11:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-Lin-packet-timeout-error/m-p/1471447#M15870</guid>
      <dc:creator>kalajiao</dc:creator>
      <dc:date>2022-06-09T11:41:16Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 Lin packet timeout error</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-Lin-packet-timeout-error/m-p/1477429#M16016</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I tried with below option and it seems it receives/sends frames upon SW2 press.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1655812433333.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/184036i0E82840BC6EF4A10/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1655812433333.png" alt="PetrS_0-1655812433333.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1655812433333.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 11:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-Lin-packet-timeout-error/m-p/1477429#M16016</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-06-21T11:54:22Z</dc:date>
    </item>
  </channel>
</rss>