<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Problem with load the program s32k3</title>
    <link>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1464721#M15669</link>
    <description>&lt;P&gt;Hi Luka ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The software we think is not the problem because we did nothing before connect to JTAG.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We check with a thermal camera and we detect that we have a small hot point in the microchip so we think that the micro have a short circuit&lt;/P&gt;</description>
    <pubDate>Thu, 26 May 2022 10:59:12 GMT</pubDate>
    <dc:creator>Miki849</dc:creator>
    <dc:date>2022-05-26T10:59:12Z</dc:date>
    <item>
      <title>Problem with load the program s32k3</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1461404#M15560</link>
      <description>&lt;P&gt;Hi everybody,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Today, I found a problem with my evaluation board . when i try program it , the s32 Ds give me the next error:&lt;/P&gt;&lt;P&gt;Error in final launch sequence:&lt;/P&gt;&lt;P&gt;Failed to execute MI command:&lt;BR /&gt;-exec-run&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Error creating process C:\Users\mgarcia\workspaceS32DS.3.4\Siul2_Dio_ToggleLed_S32K344\Debug_FLASH\Siul2_Dio_ToggleLed_S32K344.elf, (error 193).&lt;BR /&gt;Failed to execute MI command:&lt;BR /&gt;-exec-run&lt;BR /&gt;Error message from debugger back end:&lt;BR /&gt;Error creating process C:\Users\mgarcia\workspaceS32DS.3.4\Siul2_Dio_ToggleLed_S32K344\Debug_FLASH\Siul2_Dio_ToggleLed_S32K344.elf, (error 193).&lt;BR /&gt;Error creating process C:\Users\mgarcia\workspaceS32DS.3.4\Siul2_Dio_ToggleLed_S32K344\Debug_FLASH\Siul2_Dio_ToggleLed_S32K344.elf, (error 193).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use the multilink programmer :&amp;nbsp;&lt;A href="https://es.rs-online.com/web/p/depuradores-y-emuladores-en-circuito/2194676?cm_mmc=ES-PLA-DS3A-_-google-_-CSS_ES_ES_Semiconductores_Whoop-_-(ES:Whoop!)+Depuradores+y+Emuladores+en+Circuito-_-2194676&amp;amp;matchtype=&amp;amp;pla-296653389336&amp;amp;gclid=Cj0KCQjw-JyUBhCuARIsANUqQ_K1Hh20o8hMU--vXuha4tNmfimKtRFcrkFPXvJrMhTFNaxQTErFmCUaAnX7EALw_wcB&amp;amp;gclsrc=aw.ds" target="_blank"&gt;https://es.rs-online.com/web/p/depuradores-y-emuladores-en-circuito/2194676?cm_mmc=ES-PLA-DS3A-_-google-_-CSS_ES_ES_Semiconductores_Whoop-_-(ES:Whoop!)+Depuradores+y+Emuladores+en+Circuito-_-2194676&amp;amp;matchtype=&amp;amp;pla-296653389336&amp;amp;gclid=Cj0KCQjw-JyUBhCuARIsANUqQ_K1Hh20o8hMU--vXuha4tNmfimKtRFcrkFPXvJrMhTFNaxQTErFmCUaAnX7EALw_wcB&amp;amp;gclsrc=aw.ds&lt;/A&gt;&lt;/P&gt;&lt;P&gt;And i can use it in another board without problem, moreover the program that i try to load , i used before without problem. And i can use it in another board too.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you so much in advance.&lt;/P&gt;&lt;P&gt;Kind regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Miguel&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 08:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1461404#M15560</guid>
      <dc:creator>Miki849</dc:creator>
      <dc:date>2022-05-20T08:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with load the program s32k3</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1462149#M15592</link>
      <description>&lt;P&gt;Hi Miguel,&lt;/P&gt;
&lt;P&gt;if the same project works on another board and if the same Multilink works with another board, it points at the MCU/board. From HW point of view - did you try to measure supply voltages? Is the configuration the same (like jumpers)? Was the board handled according to ESD rules? From SW point of view - do you remember what was the last operation? Was that anything special?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 05:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1462149#M15592</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-05-23T05:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with load the program s32k3</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1464721#M15669</link>
      <description>&lt;P&gt;Hi Luka ,&amp;nbsp;&lt;/P&gt;&lt;P&gt;The software we think is not the problem because we did nothing before connect to JTAG.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We check with a thermal camera and we detect that we have a small hot point in the microchip so we think that the micro have a short circuit&lt;/P&gt;</description>
      <pubDate>Thu, 26 May 2022 10:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-load-the-program-s32k3/m-p/1464721#M15669</guid>
      <dc:creator>Miki849</dc:creator>
      <dc:date>2022-05-26T10:59:12Z</dc:date>
    </item>
  </channel>
</rss>