<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K312 with HardFault_Handler</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-with-HardFault-Handler/m-p/1464682#M15666</link>
    <description>&lt;P&gt;I have a project on S32K312 (using EB tresos to configure and makefile to build and run). When I run program in debug mode,&amp;nbsp; But sometime program got hard fault, so I need to flash another project build on CT before this project&amp;nbsp;it works well. I realize that in debug mode when I press RESET button,&amp;nbsp;program run from Reset_Handler to main, and in main function, it run over some steps then go to the HardFault_Handler (maybe until the line regard to pin, port, register of chip).&lt;/P&gt;
&lt;P&gt;So what reason I encounter ? Can you help me to fix it. Or can I have a idea to trace this problem.&lt;/P&gt;
&lt;P&gt;Thank you !&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jun 2022 10:44:50 GMT</pubDate>
    <dc:creator>AnhNguyenDuc</dc:creator>
    <dc:date>2022-06-09T10:44:50Z</dc:date>
    <item>
      <title>S32K312 with HardFault_Handler</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-with-HardFault-Handler/m-p/1464682#M15666</link>
      <description>&lt;P&gt;I have a project on S32K312 (using EB tresos to configure and makefile to build and run). When I run program in debug mode,&amp;nbsp; But sometime program got hard fault, so I need to flash another project build on CT before this project&amp;nbsp;it works well. I realize that in debug mode when I press RESET button,&amp;nbsp;program run from Reset_Handler to main, and in main function, it run over some steps then go to the HardFault_Handler (maybe until the line regard to pin, port, register of chip).&lt;/P&gt;
&lt;P&gt;So what reason I encounter ? Can you help me to fix it. Or can I have a idea to trace this problem.&lt;/P&gt;
&lt;P&gt;Thank you !&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 10:44:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-with-HardFault-Handler/m-p/1464682#M15666</guid>
      <dc:creator>AnhNguyenDuc</dc:creator>
      <dc:date>2022-06-09T10:44:50Z</dc:date>
    </item>
  </channel>
</rss>