<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: error about burn the program into board when use different debuggers in S32K</title>
    <link>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1462600#M15612</link>
    <description>&lt;P&gt;hello&amp;nbsp;@&lt;SPAN&gt;Daniel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I used S32K344 MCU. I used trace32 to burn program into board w&lt;/SPAN&gt;hen the board is powered on for the first time.&amp;nbsp;&lt;SPAN&gt;Debugger display "bus error at address APB:0x8000AFE0".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is another question is that why I deleted many source to compile project，trace32 “list source” function is ok. If not to delete, the function can't work. When I add a huge array into the project deleted many source. The function“list source”&amp;nbsp; is also not ok. Can you tell me why?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Looking forward to you help!&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 23 May 2022 16:11:57 GMT</pubDate>
    <dc:creator>Xjh193</dc:creator>
    <dc:date>2022-05-23T16:11:57Z</dc:date>
    <item>
      <title>error about burn the program into board when use different debuggers</title>
      <link>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1459928#M15517</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Fault Occurrence Scenario:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;different debuggers were used alternately to burn the program without powerdown. debuggers are PE debugger and trace32 debugger.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Fault description :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1 PE cannot&amp;nbsp;&lt;SPAN&gt;connect to target board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2 trace32 display error "running locked up".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Looking forward to your help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 10:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1459928#M15517</guid>
      <dc:creator>Xjh193</dc:creator>
      <dc:date>2022-05-18T10:01:30Z</dc:date>
    </item>
    <item>
      <title>Re: error about burn the program into board when use different debuggers</title>
      <link>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1460842#M15550</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181697"&gt;@Xjh193&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You did not specify the MCU.&lt;/P&gt;
&lt;P&gt;Are there any details about the errors provided by the debuggers?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 19 May 2022 11:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1460842#M15550</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-05-19T11:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: error about burn the program into board when use different debuggers</title>
      <link>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1462600#M15612</link>
      <description>&lt;P&gt;hello&amp;nbsp;@&lt;SPAN&gt;Daniel.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I used S32K344 MCU. I used trace32 to burn program into board w&lt;/SPAN&gt;hen the board is powered on for the first time.&amp;nbsp;&lt;SPAN&gt;Debugger display "bus error at address APB:0x8000AFE0".&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is another question is that why I deleted many source to compile project，trace32 “list source” function is ok. If not to delete, the function can't work. When I add a huge array into the project deleted many source. The function“list source”&amp;nbsp; is also not ok. Can you tell me why?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Looking forward to you help!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 May 2022 16:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1462600#M15612</guid>
      <dc:creator>Xjh193</dc:creator>
      <dc:date>2022-05-23T16:11:57Z</dc:date>
    </item>
    <item>
      <title>Re: error about burn the program into board when use different debuggers</title>
      <link>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1463055#M15624</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181697"&gt;@Xjh193&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;What program/examples are you trying to flash?&lt;/P&gt;&lt;P&gt;Can you use the latest RTD RTM 2.0.0 examples from S32DS 3.4?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 08:34:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/error-about-burn-the-program-into-board-when-use-different/m-p/1463055#M15624</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-05-24T08:34:49Z</dc:date>
    </item>
  </channel>
</rss>