<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: ADC_Multiple_Channel with DMA</title>
    <link>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461579#M15571</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;through this example only I have implemented but I have used only PDB0,ADC0 channels. Every thing is same but not able to identify the problem exactly.&lt;/P&gt;</description>
    <pubDate>Fri, 20 May 2022 11:17:35 GMT</pubDate>
    <dc:creator>Bhuvana</dc:creator>
    <dc:date>2022-05-20T11:17:35Z</dc:date>
    <item>
      <title>ADC_Multiple_Channel with DMA</title>
      <link>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461349#M15558</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Through DMA I'm reading adc channel 1st its working fine but in run time if I change value only 1st 8 channel is reading the correct data in remaining channels I'm not able to read the data its showing same old data only&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 06:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461349#M15558</guid>
      <dc:creator>Bhuvana</dc:creator>
      <dc:date>2022-05-20T06:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: ADC_Multiple_Channel with DMA</title>
      <link>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461503#M15564</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;could one of below examples be useful?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-trigger-DMA-ISR-S32DS/ta-p/1103221" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-trigger-DMA-ISR-S32DS/ta-p/1103221&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 09:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461503#M15564</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-05-20T09:19:23Z</dc:date>
    </item>
    <item>
      <title>Re: ADC_Multiple_Channel with DMA</title>
      <link>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461579#M15571</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;through this example only I have implemented but I have used only PDB0,ADC0 channels. Every thing is same but not able to identify the problem exactly.&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 11:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1461579#M15571</guid>
      <dc:creator>Bhuvana</dc:creator>
      <dc:date>2022-05-20T11:17:35Z</dc:date>
    </item>
    <item>
      <title>Re: ADC_Multiple_Channel with DMA</title>
      <link>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1463053#M15623</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;seems it is due to sample time is set to be inconsistent with PDB setting. Change ADC0 clock to run from FIRC DIV2 in Clocks tool. Set sample time = 14 in ADC component. Finally if 14 samples are read by DMA, then config 14 pretriggers in&amp;nbsp;PDB0_init.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 May 2022 08:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC-Multiple-Channel-with-DMA/m-p/1463053#M15623</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-05-24T08:34:44Z</dc:date>
    </item>
  </channel>
</rss>