<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K3X4EVB-Q172 Debug Connector cable</title>
    <link>https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-Debug-Connector-cable/m-p/1454178#M15293</link>
    <description>&lt;P&gt;I want to connect a Segger debugger (&lt;SPAN&gt;0.1" 20-pin Standard ARM debug connector) to the&amp;nbsp;S32K3X4EVB-Q172 evalution board. This board only has a 20-pin Cortex Debug ETM+Trace connector (0.05'' 20-pin FTSH header).&lt;BR /&gt;&lt;BR /&gt;Can you suggest an adapter/cable that I can use for this? The adapter from Segger (&lt;A href="https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/" target="_blank"&gt;https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/&lt;/A&gt;) does match the pin-out but contains a dead-pin (they also call it a 19-pin adapter):&lt;IMG src="https://nl.mouser.com/images/seggermicrocontroller/hd/inhouse_jlink19pincortexmadapter_t.jpg" border="0" width="291" height="225" /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Which cable/adapter can I use to connect a debugger to the S32K3X4EVB-Q172?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 06 May 2022 10:40:15 GMT</pubDate>
    <dc:creator>joohau</dc:creator>
    <dc:date>2022-05-06T10:40:15Z</dc:date>
    <item>
      <title>S32K3X4EVB-Q172 Debug Connector cable</title>
      <link>https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-Debug-Connector-cable/m-p/1454178#M15293</link>
      <description>&lt;P&gt;I want to connect a Segger debugger (&lt;SPAN&gt;0.1" 20-pin Standard ARM debug connector) to the&amp;nbsp;S32K3X4EVB-Q172 evalution board. This board only has a 20-pin Cortex Debug ETM+Trace connector (0.05'' 20-pin FTSH header).&lt;BR /&gt;&lt;BR /&gt;Can you suggest an adapter/cable that I can use for this? The adapter from Segger (&lt;A href="https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/" target="_blank"&gt;https://www.segger.com/products/debug-probes/j-link/accessories/adapters/19-pin-cortex-m-adapter/&lt;/A&gt;) does match the pin-out but contains a dead-pin (they also call it a 19-pin adapter):&lt;IMG src="https://nl.mouser.com/images/seggermicrocontroller/hd/inhouse_jlink19pincortexmadapter_t.jpg" border="0" width="291" height="225" /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Which cable/adapter can I use to connect a debugger to the S32K3X4EVB-Q172?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 06 May 2022 10:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-Debug-Connector-cable/m-p/1454178#M15293</guid>
      <dc:creator>joohau</dc:creator>
      <dc:date>2022-05-06T10:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3X4EVB-Q172 Debug Connector cable</title>
      <link>https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-Debug-Connector-cable/m-p/1461651#M15578</link>
      <description>&lt;P&gt;Hi Joost,&lt;/P&gt;
&lt;P&gt;this should work, you just need to remove the dead-pin to be able to plug it in.&lt;/P&gt;
&lt;P&gt;I use something similar (LA-3500 + LA7844 + these converters LA-3770) and there was also the same dead-pin which I removed:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1653050964717.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/180447iA75A79B24B46EDC3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1653050964717.png" alt="lukaszadrapa_0-1653050964717.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 12:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3X4EVB-Q172-Debug-Connector-cable/m-p/1461651#M15578</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-05-20T12:50:52Z</dc:date>
    </item>
  </channel>
</rss>