<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 FLEXNVM</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1452810#M15260</link>
    <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I&amp;nbsp;use the bootloader in AN12218 on a S32K144.It works normally.But,It does not work when I using UART interrupt rx.UART can not receive data.May be something wrong with the flexnvm used code flash.Bootloader can find the interrupr table.What should I do? I need your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 04 May 2022 15:40:04 GMT</pubDate>
    <dc:creator>gangzhou</dc:creator>
    <dc:date>2022-05-04T15:40:04Z</dc:date>
    <item>
      <title>S32K144 FLEXNVM</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1452810#M15260</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I&amp;nbsp;use the bootloader in AN12218 on a S32K144.It works normally.But,It does not work when I using UART interrupt rx.UART can not receive data.May be something wrong with the flexnvm used code flash.Bootloader can find the interrupr table.What should I do? I need your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 May 2022 15:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1452810#M15260</guid>
      <dc:creator>gangzhou</dc:creator>
      <dc:date>2022-05-04T15:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FLEXNVM</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1461576#M15569</link>
      <description>&lt;P&gt;Hi Gang,&lt;/P&gt;
&lt;P&gt;it's not clear to me. Are you modifying the bootloader? Or do you mean that user application is not working? Is the application working if it is executed without bootloader?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 11:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1461576#M15569</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-05-20T11:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FLEXNVM</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1465836#M15705</link>
      <description>&lt;P&gt;Thank you for your reply.I modified the bootloader.Used&amp;nbsp;&lt;SPAN&gt;UART interrupt receive data.But ,Bootloader did not work,because the&amp;nbsp; UART interrupt could not enter.May be something wrong while placing code data in address 0x10000000 without changing the vector&amp;nbsp; address.What should I do?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 29 May 2022 06:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1465836#M15705</guid>
      <dc:creator>gangzhou</dc:creator>
      <dc:date>2022-05-29T06:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FLEXNVM</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1465943#M15710</link>
      <description>&lt;P&gt;I would check: if VTOR register points to your vector table, if the interrupt is enabled and if priority is configured appropriately in NVIC, if the interrupt in LPUART module is enabled and if interrupt flag is set. All these conditions should be met to trigger the interrupt.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 30 May 2022 04:47:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FLEXNVM/m-p/1465943#M15710</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-05-30T04:47:13Z</dc:date>
    </item>
  </channel>
</rss>