<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k144 CAN example in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610318#M152</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you have EVB board powered by external supply into J16? The SBC chip is powered by this external 12V source.&lt;/P&gt;&lt;P&gt;I tested those demos on 2 EVB and it is working well. There is a same behavior without external power supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Oct 2016 10:21:57 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2016-10-07T10:21:57Z</dc:date>
    <item>
      <title>s32k144 CAN example</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610317#M151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to get CAN to work with the evaluation board for S32K144.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have downloaded Design studio and imported examples CAN_MASTER and CAN_SLAVE, (the use&amp;nbsp;S32_SDK_EAR_0.8.1)&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;They build and flash ok.&lt;/P&gt;&lt;P&gt;But I can't see any CAN communication.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have measured TP20 for sbc_can_rx and TP21 for sbc_can_tx.&lt;/P&gt;&lt;P&gt;TP20 is always low, and TP21 is always high.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What am I missing here?&lt;/P&gt;&lt;P&gt;Think the examples should work out of the box.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2016 07:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610317#M151</guid>
      <dc:creator>tommysvensson</dc:creator>
      <dc:date>2016-10-06T07:46:28Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 CAN example</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610318#M152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you have EVB board powered by external supply into J16? The SBC chip is powered by this external 12V source.&lt;/P&gt;&lt;P&gt;I tested those demos on 2 EVB and it is working well. There is a same behavior without external power supply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 10:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610318#M152</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-10-07T10:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 CAN example</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610319#M153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I have downloaded the S32DS for ARM v2.0.&amp;nbsp; But I could not find the CAN_MASTER and CAN_SLAVE example in the installed SDK's. I could not find any example for CAN master-slave communication in my folders.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you tell me where am I going wrong in this?&lt;/P&gt;&lt;P&gt;Any pointers would be helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. I wanted to test a simple CAN communication between two S32K144 boards.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ravi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2019 00:46:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-CAN-example/m-p/610319#M153</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2019-02-14T00:46:38Z</dc:date>
    </item>
  </channel>
</rss>