<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Double bit error detection in SRAM_L</title>
    <link>https://community.nxp.com/t5/S32K/Double-bit-error-detection-in-SRAM-L/m-p/1450419#M15178</link>
    <description>&lt;P&gt;I have enabled ERM-&amp;gt;CR0[ESCIE0], ERM-&amp;gt;CR0[ENCIE0], ERM-&amp;gt;CR0[ESCIE1],ERM-&amp;gt;CR0[ENCIE1] and corresponding register in S32k146 as per S32KReferenceManual. Using EIM,&lt;BR /&gt;injected Single bit error in SRAM_L, getting notification in ERM_single_fault_IRQHandler with ERM-&amp;gt;SR0 as 0x80000000&lt;BR /&gt;injected Single bit error in SRAM_U, getting notification in ERM_single_fault_IRQHandler with ERM-&amp;gt;SR0 as 0x40000000&lt;BR /&gt;injected Double bit error in SRAM_U, getting notification in ERM_double_fault_IRQHandler with ERM-&amp;gt;SR0 as 0x04000000.&lt;BR /&gt;But while I inject Double bit error in SRAM_L, getting system reset. Not sure why reset in SRAM_U Double bit error injection.&lt;BR /&gt;My requirement is to capture both single bit &amp;amp; double bit error in SRAM and move the system to Safe state. is it feasible to implement?&lt;/P&gt;</description>
    <pubDate>Thu, 28 Apr 2022 05:30:52 GMT</pubDate>
    <dc:creator>Sankar_saba</dc:creator>
    <dc:date>2022-04-28T05:30:52Z</dc:date>
    <item>
      <title>Double bit error detection in SRAM_L</title>
      <link>https://community.nxp.com/t5/S32K/Double-bit-error-detection-in-SRAM-L/m-p/1450419#M15178</link>
      <description>&lt;P&gt;I have enabled ERM-&amp;gt;CR0[ESCIE0], ERM-&amp;gt;CR0[ENCIE0], ERM-&amp;gt;CR0[ESCIE1],ERM-&amp;gt;CR0[ENCIE1] and corresponding register in S32k146 as per S32KReferenceManual. Using EIM,&lt;BR /&gt;injected Single bit error in SRAM_L, getting notification in ERM_single_fault_IRQHandler with ERM-&amp;gt;SR0 as 0x80000000&lt;BR /&gt;injected Single bit error in SRAM_U, getting notification in ERM_single_fault_IRQHandler with ERM-&amp;gt;SR0 as 0x40000000&lt;BR /&gt;injected Double bit error in SRAM_U, getting notification in ERM_double_fault_IRQHandler with ERM-&amp;gt;SR0 as 0x04000000.&lt;BR /&gt;But while I inject Double bit error in SRAM_L, getting system reset. Not sure why reset in SRAM_U Double bit error injection.&lt;BR /&gt;My requirement is to capture both single bit &amp;amp; double bit error in SRAM and move the system to Safe state. is it feasible to implement?&lt;/P&gt;</description>
      <pubDate>Thu, 28 Apr 2022 05:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Double-bit-error-detection-in-SRAM-L/m-p/1450419#M15178</guid>
      <dc:creator>Sankar_saba</dc:creator>
      <dc:date>2022-04-28T05:30:52Z</dc:date>
    </item>
  </channel>
</rss>