<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32k3 FreeRTOS UART RX Callback Information</title>
    <link>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1450127#M15170</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use one callback function to receive RX events using all 4 UART channels on the S32k3X4EVB-Q257.&lt;/P&gt;&lt;P&gt;I then need to determine which channel the message came in on.&lt;/P&gt;&lt;P&gt;Has anyone done this? Possibly using the void userData pointer parameter?&lt;/P&gt;&lt;P&gt;Or any other way.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I cannot use separate callbacks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;-Sean L&lt;/P&gt;</description>
    <pubDate>Wed, 27 Apr 2022 20:47:40 GMT</pubDate>
    <dc:creator>SL239</dc:creator>
    <dc:date>2022-04-27T20:47:40Z</dc:date>
    <item>
      <title>S32k3 FreeRTOS UART RX Callback Information</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1450127#M15170</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use one callback function to receive RX events using all 4 UART channels on the S32k3X4EVB-Q257.&lt;/P&gt;&lt;P&gt;I then need to determine which channel the message came in on.&lt;/P&gt;&lt;P&gt;Has anyone done this? Possibly using the void userData pointer parameter?&lt;/P&gt;&lt;P&gt;Or any other way.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I cannot use separate callbacks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;-Sean L&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 20:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1450127#M15170</guid>
      <dc:creator>SL239</dc:creator>
      <dc:date>2022-04-27T20:47:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3 FreeRTOS UART RX Callback Information</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1451226#M15214</link>
      <description>&lt;P&gt;Hi Sean,&lt;/P&gt;
&lt;P&gt;I can see in the callback typedef that there's HwInstance parameter, so you should have information about the channel:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1651224171772.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/178422i0A27A6866B7DA06C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1651224171772.png" alt="lukaszadrapa_0-1651224171772.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 09:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1451226#M15214</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-04-29T09:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3 FreeRTOS UART RX Callback Information</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1451391#M15218</link>
      <description>&lt;P&gt;Thanks for your reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to accomplish this by using the HwInstance, and the Event type.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 29 Apr 2022 14:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-FreeRTOS-UART-RX-Callback-Information/m-p/1451391#M15218</guid>
      <dc:creator>SL239</dc:creator>
      <dc:date>2022-04-29T14:33:48Z</dc:date>
    </item>
  </channel>
</rss>