<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K144 FlexTimer(FTM)Module function consultation</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FlexTimer-FTM-Module-function-consultation/m-p/1447891#M15080</link>
    <description>&lt;P&gt;I'm using the FTM module of s32k144. I have a few questions. I want to give full play to the performance of s32k144 as much as possible, so the following questions are very important to me.I hope someone who knows this knowledge can help answer them.Thank you very much！&lt;/P&gt;&lt;P&gt;1.I want to use &lt;STRONG&gt;channel 0 of FTM0&lt;/STRONG&gt; module to collect &lt;STRONG&gt;frequency and duty cycle&lt;/STRONG&gt; at the same time. Can this function be realized? There is no response sample code for reference.&lt;/P&gt;&lt;P&gt;2.I want to use &lt;STRONG&gt;channel 0 of FTM0 module&lt;/STRONG&gt; as&lt;STRONG&gt; PWM input signal acquisition&lt;/STRONG&gt; and &lt;STRONG&gt;channel 3 as PWM output.&lt;/STRONG&gt; Can this be realized? Are there any engineering examples of response for reference?&lt;/P&gt;</description>
    <pubDate>Fri, 22 Apr 2022 14:22:47 GMT</pubDate>
    <dc:creator>fanshichencao</dc:creator>
    <dc:date>2022-04-22T14:22:47Z</dc:date>
    <item>
      <title>S32K144 FlexTimer(FTM)Module function consultation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexTimer-FTM-Module-function-consultation/m-p/1447891#M15080</link>
      <description>&lt;P&gt;I'm using the FTM module of s32k144. I have a few questions. I want to give full play to the performance of s32k144 as much as possible, so the following questions are very important to me.I hope someone who knows this knowledge can help answer them.Thank you very much！&lt;/P&gt;&lt;P&gt;1.I want to use &lt;STRONG&gt;channel 0 of FTM0&lt;/STRONG&gt; module to collect &lt;STRONG&gt;frequency and duty cycle&lt;/STRONG&gt; at the same time. Can this function be realized? There is no response sample code for reference.&lt;/P&gt;&lt;P&gt;2.I want to use &lt;STRONG&gt;channel 0 of FTM0 module&lt;/STRONG&gt; as&lt;STRONG&gt; PWM input signal acquisition&lt;/STRONG&gt; and &lt;STRONG&gt;channel 3 as PWM output.&lt;/STRONG&gt; Can this be realized? Are there any engineering examples of response for reference?&lt;/P&gt;</description>
      <pubDate>Fri, 22 Apr 2022 14:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexTimer-FTM-Module-function-consultation/m-p/1447891#M15080</guid>
      <dc:creator>fanshichencao</dc:creator>
      <dc:date>2022-04-22T14:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FlexTimer(FTM)Module function consultation</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexTimer-FTM-Module-function-consultation/m-p/1448149#M15087</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@fanshichencao" target="_blank"&gt;Hi@fanshichencao&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; for the first question,the answer is yes,you can take a look at the demos in S32 DS, i remember there is a demo shows how to use FTM module to measure PWM frequence and duty cycles.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; for the second question,the answer is no,channels under an FTM module can only be set as input or output at the same time.&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Jim,&lt;/P&gt;</description>
      <pubDate>Sun, 24 Apr 2022 07:08:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexTimer-FTM-Module-function-consultation/m-p/1448149#M15087</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-04-24T07:08:16Z</dc:date>
    </item>
  </channel>
</rss>