<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CSEC_BOOT_MAC update fail in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1446040#M15030</link>
    <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;When updating CSEC_BOOT_MAC, CSEC_DRV_LoadKey() returned an update failure. The return value of the failure is STATUS_SEC_KEY_UPDATE_ERROR.May I ask the reason for this failure to rest&lt;/P&gt;&lt;P&gt;PS: I used the&amp;nbsp;auth key is master key.&lt;/P&gt;</description>
    <pubDate>Wed, 20 Apr 2022 03:04:46 GMT</pubDate>
    <dc:creator>wang_q4</dc:creator>
    <dc:date>2022-04-20T03:04:46Z</dc:date>
    <item>
      <title>CSEC_BOOT_MAC update fail</title>
      <link>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1446040#M15030</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;When updating CSEC_BOOT_MAC, CSEC_DRV_LoadKey() returned an update failure. The return value of the failure is STATUS_SEC_KEY_UPDATE_ERROR.May I ask the reason for this failure to rest&lt;/P&gt;&lt;P&gt;PS: I used the&amp;nbsp;auth key is master key.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 03:04:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1446040#M15030</guid>
      <dc:creator>wang_q4</dc:creator>
      <dc:date>2022-04-20T03:04:46Z</dc:date>
    </item>
    <item>
      <title>Re: CSEC_BOOT_MAC update fail</title>
      <link>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1446370#M15050</link>
      <description>&lt;P&gt;Add: using master key as the auth key, i can update other keys&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 11:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1446370#M15050</guid>
      <dc:creator>wang_q4</dc:creator>
      <dc:date>2022-04-20T11:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: CSEC_BOOT_MAC update fail</title>
      <link>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1447166#M15062</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I can't see reason for this. BOOT_MAC can be updated with knowledge of old value of BOOT_MAC or with knowledge of MASTER_ECU_KEY. Counter needs to be incremented appropriately. How do you calculate M1-M5 values? Are you sure that correct values are provided?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 21 Apr 2022 10:17:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC-BOOT-MAC-update-fail/m-p/1447166#M15062</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-04-21T10:17:35Z</dc:date>
    </item>
  </channel>
</rss>