<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RMII interface with 25MHz? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/RMII-interface-with-25MHz/m-p/1445817#M15023</link>
    <description>&lt;P&gt;I am using S32k together with a SJA1105 Ethernet switch. Between these deviced, I have inverted the Clock-Signals, so that I can not generate the 50MHz clock with the MCU.&lt;BR /&gt;I could generate 25MHz with the SJA1105.&lt;BR /&gt;&lt;BR /&gt;Is it possible to run the RMII interface with 25MHz clock?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 19 Apr 2022 13:53:52 GMT</pubDate>
    <dc:creator>FSeliger</dc:creator>
    <dc:date>2022-04-19T13:53:52Z</dc:date>
    <item>
      <title>RMII interface with 25MHz?</title>
      <link>https://community.nxp.com/t5/S32K/RMII-interface-with-25MHz/m-p/1445817#M15023</link>
      <description>&lt;P&gt;I am using S32k together with a SJA1105 Ethernet switch. Between these deviced, I have inverted the Clock-Signals, so that I can not generate the 50MHz clock with the MCU.&lt;BR /&gt;I could generate 25MHz with the SJA1105.&lt;BR /&gt;&lt;BR /&gt;Is it possible to run the RMII interface with 25MHz clock?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 19 Apr 2022 13:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RMII-interface-with-25MHz/m-p/1445817#M15023</guid>
      <dc:creator>FSeliger</dc:creator>
      <dc:date>2022-04-19T13:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: RMII interface with 25MHz?</title>
      <link>https://community.nxp.com/t5/S32K/RMII-interface-with-25MHz/m-p/1446184#M15040</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I don't think so, 50MHZ is needed for RMII mode.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 20 Apr 2022 07:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RMII-interface-with-25MHz/m-p/1446184#M15040</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-04-20T07:42:11Z</dc:date>
    </item>
  </channel>
</rss>