<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K Battery Cell Controller Evaluation Software does not build out of the box</title>
    <link>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1440852#M14849</link>
    <description>&lt;P&gt;i just downloaded the sample software for this evm&lt;/P&gt;&lt;H3&gt;RD33771CNTREVM&lt;/H3&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but the project does not build.&amp;nbsp;&lt;/P&gt;&lt;P&gt;there is duplicated symbol definition&amp;nbsp;g_lpspiState in both the uja1169.c and the mc33771c_peripheries.c .. any one from nxp can test this out?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Apr 2022 22:17:04 GMT</pubDate>
    <dc:creator>gzleng</dc:creator>
    <dc:date>2022-04-07T22:17:04Z</dc:date>
    <item>
      <title>S32K Battery Cell Controller Evaluation Software does not build out of the box</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1440852#M14849</link>
      <description>&lt;P&gt;i just downloaded the sample software for this evm&lt;/P&gt;&lt;H3&gt;RD33771CNTREVM&lt;/H3&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but the project does not build.&amp;nbsp;&lt;/P&gt;&lt;P&gt;there is duplicated symbol definition&amp;nbsp;g_lpspiState in both the uja1169.c and the mc33771c_peripheries.c .. any one from nxp can test this out?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 22:17:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1440852#M14849</guid>
      <dc:creator>gzleng</dc:creator>
      <dc:date>2022-04-07T22:17:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Battery Cell Controller Evaluation Software does not build out of the box</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1440920#M14850</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@gleng" target="_blank"&gt;Hi@gleng&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I have downloaded this demo project ,and it works fine on my side, i guess the wrong resaon duo to your IDE or RTM version is not right for this demo.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;1.Download the S32 Design Studio IDE for ARM (Version 2018.R1 is recommended).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2.I checked the RTM version ,which is&amp;nbsp;&lt;STRONG&gt;SDK_S32K1xx_13&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;so please double check your IDE or Driver version again.&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Jim,&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 01:56:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1440920#M14850</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-04-08T01:56:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K Battery Cell Controller Evaluation Software does not build out of the box</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1441562#M14881</link>
      <description>&lt;P&gt;thank you Jim for the verification.&lt;/P&gt;&lt;P&gt;i'm using the latest IDE from nxp website which is R2.2 and the SDK version is RTM 3. i would expect the toolchain to be backward compatible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;on the other hand, if you look into the two files that i mentioned, they both DO contain exactly the same variable definition, which is a violation of the C project thus it should have failed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;s32K_1xx_BCC_Eval/sources/uja_sbc/uja_1169.c line 15: lpspi_state_t g_lpspiState[LPSPI_INSTANCE_COUNT];&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;s32K_1xx_BCC_Eval/sources/mc33771c/mc33771c_peripheries.c line 53:&amp;nbsp;lpspi_state_t g_lpspiState[LPSPI_INSTANCE_COUNT];&lt;/P&gt;&lt;P&gt;there would be a linker error when linking the final elf.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;gz&lt;/P&gt;</description>
      <pubDate>Sat, 09 Apr 2022 04:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Battery-Cell-Controller-Evaluation-Software-does-not-build/m-p/1441562#M14881</guid>
      <dc:creator>gzleng</dc:creator>
      <dc:date>2022-04-09T04:13:20Z</dc:date>
    </item>
  </channel>
</rss>