<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Output Current S32K144-EVB in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438844#M14783</link>
    <description>&lt;P&gt;Thanks for the reply. Will a given GPIO port be able to source the required 20mA? I understand that collectively all the ports can source 100mA. Is there an individual pin's maximum rating due to hardware or packaging constraint? Thanks and Regards&lt;/P&gt;</description>
    <pubDate>Tue, 05 Apr 2022 11:13:00 GMT</pubDate>
    <dc:creator>asrikrishnagovind</dc:creator>
    <dc:date>2022-04-05T11:13:00Z</dc:date>
    <item>
      <title>Output Current S32K144-EVB</title>
      <link>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438290#M14755</link>
      <description>&lt;P&gt;Hello, I have a Motor Drive application, which utilizes 4 Hall Effect Sensors (5v)&amp;nbsp; to measure phase currents, and each of the sensor requires about 20mA of current typically to operate, along with an Encoder with similar requirements.&lt;/P&gt;&lt;P&gt;In the Datasheet of S32K1XX:&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/S32K-DS.pdf" target="_blank"&gt;S32K1XX: S32K1xx Data Sheet (nxp.com)&lt;/A&gt;&amp;nbsp;Page 31, it was shown that the "Output high current total for all ports is 100mA". My query is, will the Evaluation Board&amp;nbsp;S32K144-EVB be able to provide the current requirements of these sensors? Thanks and Regards&lt;/P&gt;</description>
      <pubDate>Mon, 04 Apr 2022 11:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438290#M14755</guid>
      <dc:creator>asrikrishnagovind</dc:creator>
      <dc:date>2022-04-04T11:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: Output Current S32K144-EVB</title>
      <link>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438826#M14781</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193481"&gt;@asrikrishnagovind&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The MCU can provide combined 100mA at GPIOs (Output HIGH) as you mentioned.&lt;/P&gt;
&lt;P&gt;But the MCU is powered by the SBC UJA1169&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1649155600400.png" style="width: 851px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/175899iDEB9D07DA178BE3E/image-dimensions/851x447?v=v2" width="851" height="447" role="button" title="danielmartynek_0-1649155600400.png" alt="danielmartynek_0-1649155600400.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1649155600400.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/UJA1169.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/UJA1169.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1649155723671.png" style="width: 824px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/175900i7C111BF5F55DE884/image-dimensions/824x452?v=v2" width="824" height="452" role="button" title="danielmartynek_1-1649155723671.png" alt="danielmartynek_1-1649155723671.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_1-1649155723671.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 05 Apr 2022 10:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438826#M14781</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-04-05T10:49:41Z</dc:date>
    </item>
    <item>
      <title>Re: Output Current S32K144-EVB</title>
      <link>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438844#M14783</link>
      <description>&lt;P&gt;Thanks for the reply. Will a given GPIO port be able to source the required 20mA? I understand that collectively all the ports can source 100mA. Is there an individual pin's maximum rating due to hardware or packaging constraint? Thanks and Regards&lt;/P&gt;</description>
      <pubDate>Tue, 05 Apr 2022 11:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438844#M14783</guid>
      <dc:creator>asrikrishnagovind</dc:creator>
      <dc:date>2022-04-05T11:13:00Z</dc:date>
    </item>
    <item>
      <title>Re: Output Current S32K144-EVB</title>
      <link>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438849#M14785</link>
      <description>&lt;P&gt;Normal GPIOs can source 5mA at max voltage drop VDD - 0.8V at the output pin.&lt;/P&gt;
&lt;P&gt;GPIO-HD pins (if DSE = 1) can source 20mA at max drop of 0.8V.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1649157796494.png" style="width: 716px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/175905i72FDDC27EF97AE39/image-dimensions/716x562?v=v2" width="716" height="562" role="button" title="danielmartynek_0-1649157796494.png" alt="danielmartynek_0-1649157796494.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielmartynek_0-1649157796494.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In other words, if the load is 20mA per pin / sensor, the sensor will not be powered by 5V but by &amp;gt;= 4.2V.&lt;/P&gt;
&lt;P&gt;The sensors can be powered from the 5V generated by the SBC directly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 05 Apr 2022 13:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Output-Current-S32K144-EVB/m-p/1438849#M14785</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2022-04-05T13:25:47Z</dc:date>
    </item>
  </channel>
</rss>