<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RappID Bootloader S32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708280#M1461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/koehlerl"&gt;koehlerl&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on my experience with S32K144 and i can confirm the RAppID_BL works with UART1 interface. I'm using the OpenSDA microUSB connector from S32K144 EVB to program the elf into flash/ram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For that you will need to flash the RBF file first (using S32DS). Have you done that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Aug 2017 09:06:46 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2017-08-31T09:06:46Z</dc:date>
    <item>
      <title>RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708277#M1458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;witch UART use the RappID Bootloader in the S32K144 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 06:08:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708277#M1458</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2017-08-28T06:08:23Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708278#M1459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lutz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the LPUART2 (pins PTD7/TX and PTD6/RX) is used with baudrate 115200bps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 08:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708278#M1459</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-08-31T08:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708279#M1460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but with LPUART2 I can’t connect to the PC RappID BL Tool and the trace window is empty .&lt;/P&gt;&lt;P&gt;With the LPUART0 I get the trace see attachment. But it don’t works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Lutz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: PetrS &lt;/P&gt;&lt;P&gt;Gesendet: Donnerstag, 31. August 2017 10:21&lt;/P&gt;&lt;P&gt;An: Köhler, Lutz &amp;lt;lutz.koehler@acd-antriebstechnik.de&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Re: RappID Bootloader S32K144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: RappID Bootloader S32K144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Petr Stancik&amp;lt;https://community.nxp.com/people/PetrS?et=watches.email.thread&amp;gt; in S32K - View the full discussion&amp;lt;https://community.nxp.com/message/938684?commentID=938684&amp;amp;et=watches.email.thread#comment-938684&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 08:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708279#M1460</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2017-08-31T08:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708280#M1461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/koehlerl"&gt;koehlerl&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on my experience with S32K144 and i can confirm the RAppID_BL works with UART1 interface. I'm using the OpenSDA microUSB connector from S32K144 EVB to program the elf into flash/ram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For that you will need to flash the RBF file first (using S32DS). Have you done that ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 09:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708280#M1461</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-08-31T09:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708281#M1462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the S32K144 EVB. I have flashed the rbf file first. But I can’t connect with the RappID BL tool.&lt;/P&gt;&lt;P&gt;The trace window of RappID BL Tool is empty an then after timeout the Error message comes:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are different kinds of the rbf file for the s32K144 CPU?&lt;/P&gt;&lt;P&gt;BR Lutz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: dumitru-daniel.popa &lt;/P&gt;&lt;P&gt;Gesendet: Donnerstag, 31. August 2017 11:07&lt;/P&gt;&lt;P&gt;An: Köhler, Lutz &amp;lt;lutz.koehler@acd-antriebstechnik.de&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Re: RappID Bootloader S32K144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: RappID Bootloader S32K144&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from dumitru-daniel.popa&amp;lt;https://community.nxp.com/people/dumitru-daniel.popa?et=watches.email.thread&amp;gt; in S32K - View the full discussion&amp;lt;https://community.nxp.com/message/938696?commentID=938696&amp;amp;et=watches.email.thread#comment-938696&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 09:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708281#M1462</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2017-08-31T09:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708282#M1463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lutz,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are different versions of RAppID_BL.exe and different versions of RBF files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using bootloader version 1.6.5.1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28244iFDF89C2A40F546EC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And the RBL attached and is working fine via the micro-usb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a snapshot programming the S32K144EVB-Q100&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/28203i01F061CE4FE91321/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 14:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708282#M1463</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-08-31T14:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708283#M1464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the version you have works on cut1 device (0N77P) not on cut2(&lt;SPAN style="font-size: 11.0pt;"&gt;0N47T&lt;/SPAN&gt;). Attached is the one that works on cut2 MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Sep 2017 07:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708283#M1464</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-09-01T07:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708284#M1465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Petr,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's strange. I have only cut2(0N47T) and it works fine.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Sep 2017 08:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708284#M1465</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-09-01T08:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708285#M1466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after double check, and several power down/up yours is working too. Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway I have bootloader version 1.6.7.35&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27455iBC3A4B5C2B9A5D78/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and the RBF file included works on cut1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Sep 2017 08:12:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708285#M1466</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-09-01T08:12:38Z</dc:date>
    </item>
    <item>
      <title>Re: RappID Bootloader S32K144</title>
      <link>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708286#M1467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a rbf file for the S32k144 cut2 0N47T where UART0 is used instead of UART2.&lt;/P&gt;&lt;P&gt;Where can I get such a rbf file or is it possible to get the source code to make my one rbf file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 08:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RappID-Bootloader-S32K144/m-p/708286#M1467</guid>
      <dc:creator>koehlerl</dc:creator>
      <dc:date>2017-09-06T08:56:13Z</dc:date>
    </item>
  </channel>
</rss>