<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 SWD&amp;JTAG Problem in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-SWD-JTAG-Problem/m-p/708231#M1457</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I know what is going on:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;JTAG supports Boundary Scan (used to check circuit board connections).&amp;nbsp; SWD (Serial Wire Debug) does not.&lt;/LI&gt;&lt;LI&gt;Other than this - SWD performance is more or less the same as JTAG.&amp;nbsp; In Keil uVision, SWD = SW.&lt;/LI&gt;&lt;LI&gt;SWD is only 2 signals compared to 4 or 5 on JTAG.&amp;nbsp; So - motivated to use SWD only to save pins.&lt;/LI&gt;&lt;LI&gt;The chip designer (NXP in this case) can select JTAG OR SWD or both.&amp;nbsp; Cortex-M0 must pick one.&lt;/LI&gt;&lt;LI&gt;Keil uVision detects both JTAG and SWD in the SWJ macrocell - but JTAG cannot connect to the Cortex-M4 CoreSight debug module.&amp;nbsp; SWD can.&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;&lt;STRONG&gt;So:&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt; I think the NXP designer uses JTAG only for Boundary Scan and not for debugging.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;&lt;EM&gt;So:&amp;nbsp;&lt;/EM&gt;&lt;/STRONG&gt; Use SWD for debugging.&amp;nbsp; This will not cause any problems.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE:&lt;/STRONG&gt;&amp;nbsp; Using the S32K-144 on-board OpenSDA in CMSIS-DAP mode: only SWD works - JTAG returns an RDDI error.&amp;nbsp; I think it is common for CMSIS-DAP implementations to use only SWD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The next time I bump into a NXP designer I will ask him/her for confirmation...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bob Boys&lt;/P&gt;&lt;P&gt;Arm/Keil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Aug 2017 02:55:06 GMT</pubDate>
    <dc:creator>robertboys</dc:creator>
    <dc:date>2017-08-30T02:55:06Z</dc:date>
    <item>
      <title>S32K144 SWD&amp;JTAG Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-SWD-JTAG-Problem/m-p/708230#M1456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; IN S32K144 development,I found that if use JLINK to program chip ,the software(KEIL/IAR) only can found SWD device,the JTAG device can not use.So I want to know S32K144 could support both SWD/JTAG,or only can support SWD.Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 06:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-SWD-JTAG-Problem/m-p/708230#M1456</guid>
      <dc:creator>simonliu</dc:creator>
      <dc:date>2017-08-28T06:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 SWD&amp;JTAG Problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-SWD-JTAG-Problem/m-p/708231#M1457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I know what is going on:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;JTAG supports Boundary Scan (used to check circuit board connections).&amp;nbsp; SWD (Serial Wire Debug) does not.&lt;/LI&gt;&lt;LI&gt;Other than this - SWD performance is more or less the same as JTAG.&amp;nbsp; In Keil uVision, SWD = SW.&lt;/LI&gt;&lt;LI&gt;SWD is only 2 signals compared to 4 or 5 on JTAG.&amp;nbsp; So - motivated to use SWD only to save pins.&lt;/LI&gt;&lt;LI&gt;The chip designer (NXP in this case) can select JTAG OR SWD or both.&amp;nbsp; Cortex-M0 must pick one.&lt;/LI&gt;&lt;LI&gt;Keil uVision detects both JTAG and SWD in the SWJ macrocell - but JTAG cannot connect to the Cortex-M4 CoreSight debug module.&amp;nbsp; SWD can.&lt;/LI&gt;&lt;LI&gt;&lt;EM&gt;&lt;STRONG&gt;So:&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt; I think the NXP designer uses JTAG only for Boundary Scan and not for debugging.&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;&lt;EM&gt;So:&amp;nbsp;&lt;/EM&gt;&lt;/STRONG&gt; Use SWD for debugging.&amp;nbsp; This will not cause any problems.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE:&lt;/STRONG&gt;&amp;nbsp; Using the S32K-144 on-board OpenSDA in CMSIS-DAP mode: only SWD works - JTAG returns an RDDI error.&amp;nbsp; I think it is common for CMSIS-DAP implementations to use only SWD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The next time I bump into a NXP designer I will ask him/her for confirmation...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bob Boys&lt;/P&gt;&lt;P&gt;Arm/Keil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 02:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-SWD-JTAG-Problem/m-p/708231#M1457</guid>
      <dc:creator>robertboys</dc:creator>
      <dc:date>2017-08-30T02:55:06Z</dc:date>
    </item>
  </channel>
</rss>