<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: how could i get NxpOpenBus and the unified bootloader source code? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1432508#M14561</link>
    <description>&lt;P&gt;Hi William,&lt;/P&gt;
&lt;P&gt;&lt;A id="1584979470350697008430" class="" href="https://www.nxp.com/downloads/en/snippets-boot-code-headers-monitors/unified_bootloader_framework.zip" target="_blank" rel="noopener noreferrer"&gt;&lt;SPAN&gt;Unified Bootloader Framework&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;&lt;SPAN&gt;Unified bootloader stack based on UDS and CAN/LIN TP protocol. NxpOpenBus has been sent to you through that case.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 23 Mar 2022 09:22:34 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2022-03-23T09:22:34Z</dc:date>
    <item>
      <title>how could i get NxpOpenBus and the unified bootloader source code?</title>
      <link>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1431836#M14532</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are developing VCU with S32K, we expect to flashing based on UDSonCAN and I found a&lt;/SPAN&gt;&amp;nbsp;file named " &lt;SPAN class=""&gt;Unified bootloader user guide&lt;/SPAN&gt;&amp;nbsp;" introduced about it . But&amp;nbsp;how could i get NxpOpenBus.exe and the unified bootloader source code? &lt;SPAN&gt;I have created a ticket ,thanks a lot.&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Case: 00455919&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 22 Mar 2022 09:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1431836#M14532</guid>
      <dc:creator>William-Lee</dc:creator>
      <dc:date>2022-03-22T09:11:05Z</dc:date>
    </item>
    <item>
      <title>Re: how could i get NxpOpenBus and the unified bootloader source code?</title>
      <link>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1432508#M14561</link>
      <description>&lt;P&gt;Hi William,&lt;/P&gt;
&lt;P&gt;&lt;A id="1584979470350697008430" class="" href="https://www.nxp.com/downloads/en/snippets-boot-code-headers-monitors/unified_bootloader_framework.zip" target="_blank" rel="noopener noreferrer"&gt;&lt;SPAN&gt;Unified Bootloader Framework&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;&lt;SPAN&gt;Unified bootloader stack based on UDS and CAN/LIN TP protocol. NxpOpenBus has been sent to you through that case.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 09:22:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1432508#M14561</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-03-23T09:22:34Z</dc:date>
    </item>
    <item>
      <title>Re: how could i get NxpOpenBus and the unified bootloader source code?</title>
      <link>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1470518#M15850</link>
      <description>&lt;P&gt;Hi Robin:&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;I also use S32K to develop Bootloader, so i want&amp;nbsp;&lt;SPAN&gt;NxpOpenBus too. Could you share me one?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 09:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1470518#M15850</guid>
      <dc:creator>gangx</dc:creator>
      <dc:date>2022-06-08T09:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: how could i get NxpOpenBus and the unified bootloader source code?</title>
      <link>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1739029#M27810</link>
      <description>&lt;P&gt;I also need the NXPOpenBus.exe， could you send me one?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Oct 2023 02:11:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1739029#M27810</guid>
      <dc:creator>WenbinZ</dc:creator>
      <dc:date>2023-10-13T02:11:52Z</dc:date>
    </item>
    <item>
      <title>Re: how could i get NxpOpenBus and the unified bootloader source code?</title>
      <link>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1858244#M34880</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions.&lt;/P&gt;&lt;P&gt;1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_in", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need the reply as soon as possible since I have to send a project very soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_0-1714631712015.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276890i2608DC6DCB633FA7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_0-1714631712015.png" alt="JonAnder_Amante_0-1714631712015.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_1-1714631712034.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276891iE1BC1237E35BEBA1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_1-1714631712034.png" alt="JonAnder_Amante_1-1714631712034.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_2-1714631712036.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276892iBCED3EAF36E26127/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_2-1714631712036.png" alt="JonAnder_Amante_2-1714631712036.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_3-1714631712047.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276893iB354C5CAB3B8C4F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_3-1714631712047.png" alt="JonAnder_Amante_3-1714631712047.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_4-1714631712046.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276894iA8C41D81A2D0F23D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_4-1714631712046.png" alt="JonAnder_Amante_4-1714631712046.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jon Ander Amante Jorge&lt;/P&gt;</description>
      <pubDate>Thu, 02 May 2024 06:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/how-could-i-get-NxpOpenBus-and-the-unified-bootloader-source/m-p/1858244#M34880</guid>
      <dc:creator>JonAnder_Amante</dc:creator>
      <dc:date>2024-05-02T06:35:23Z</dc:date>
    </item>
  </channel>
</rss>