<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flexcan Recieve message in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Flexcan-Recieve-message/m-p/1432423#M14555</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this function just read out MB4, so should be called after MB4 receive a message. You should have some code which test MB4 flag if set, which indicates received message into this MB. Or could be called from interrupt if this is enabled for MB4.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 23 Mar 2022 07:03:12 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-03-23T07:03:12Z</dc:date>
    <item>
      <title>Flexcan Recieve message</title>
      <link>https://community.nxp.com/t5/S32K/Flexcan-Recieve-message/m-p/1431839#M14533</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to&amp;nbsp; transmit and receive message through CAN. I am using following part to receive message through code.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AparnaSridharan_1-1647940058222.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/174374iE2FBF8CAFEFD41F8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="AparnaSridharan_1-1647940058222.png" alt="AparnaSridharan_1-1647940058222.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;AparnaSridharan_1-1647940058222.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I am transmitting message through vechicle SPY which is not updated in CAN_recieve buffer. Also whether this function depends IFLAG value. If CAN receive depends on IFLAG value how we need to update?&lt;/P&gt;&lt;P&gt;&amp;nbsp;Also I am using CAN_recieve part of FlexCAN program for CAN 2.0 in cookbook for S32K144.&lt;/P&gt;&lt;P&gt;Please help to fix this issue. Let me know if any another information needed to fix this.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Mar 2022 09:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flexcan-Recieve-message/m-p/1431839#M14533</guid>
      <dc:creator>AparnaSridharan</dc:creator>
      <dc:date>2022-03-22T09:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan Recieve message</title>
      <link>https://community.nxp.com/t5/S32K/Flexcan-Recieve-message/m-p/1432423#M14555</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this function just read out MB4, so should be called after MB4 receive a message. You should have some code which test MB4 flag if set, which indicates received message into this MB. Or could be called from interrupt if this is enabled for MB4.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 07:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flexcan-Recieve-message/m-p/1432423#M14555</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-03-23T07:03:12Z</dc:date>
    </item>
  </channel>
</rss>