<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックuse internal reference voltage for ADC S32K14X</title>
    <link>https://community.nxp.com/t5/S32K/use-internal-reference-voltage-for-ADC-S32K14X/m-p/1426191#M14360</link>
    <description>&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;We are working with MCU S32K14X ADC and we were wondering, is there internally generated reference voltage can be used for vref in the ADC instead of using external vref ? the issue is the external supply is not &lt;SPAN&gt;stable &lt;/SPAN&gt;and we need to have &lt;SPAN&gt;stable &lt;/SPAN&gt;vref provided internally for the ADC if possible.&lt;/P&gt;&lt;P&gt;if feasible, what are the internal reference voltage options?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nader Khamess&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 13:39:44 GMT</pubDate>
    <dc:creator>naderkhamess</dc:creator>
    <dc:date>2022-03-10T13:39:44Z</dc:date>
    <item>
      <title>use internal reference voltage for ADC S32K14X</title>
      <link>https://community.nxp.com/t5/S32K/use-internal-reference-voltage-for-ADC-S32K14X/m-p/1426191#M14360</link>
      <description>&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;We are working with MCU S32K14X ADC and we were wondering, is there internally generated reference voltage can be used for vref in the ADC instead of using external vref ? the issue is the external supply is not &lt;SPAN&gt;stable &lt;/SPAN&gt;and we need to have &lt;SPAN&gt;stable &lt;/SPAN&gt;vref provided internally for the ADC if possible.&lt;/P&gt;&lt;P&gt;if feasible, what are the internal reference voltage options?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Nader Khamess&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 13:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/use-internal-reference-voltage-for-ADC-S32K14X/m-p/1426191#M14360</guid>
      <dc:creator>naderkhamess</dc:creator>
      <dc:date>2022-03-10T13:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: use internal reference voltage for ADC S32K14X</title>
      <link>https://community.nxp.com/t5/S32K/use-internal-reference-voltage-for-ADC-S32K14X/m-p/1426836#M14380</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Nader Khamess,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is no internal&amp;nbsp;reference voltage can be used as ADC VREF.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="43.6 ADC Reference Options.png" style="width: 845px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/173216iFF9322787D9B0426/image-size/large?v=v2&amp;amp;px=999" role="button" title="43.6 ADC Reference Options.png" alt="43.6 ADC Reference Options.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;There is&amp;nbsp;&lt;A href="http://Question%20about ADC bandgap voltage value" target="_self"&gt;1V&amp;nbsp;&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;&lt;A href="http://Question%20about ADC bandgap voltage value" target="_self"&gt;bandgap&lt;/A&gt;, but it's ADC input not vref.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 10:35:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/use-internal-reference-voltage-for-ADC-S32K14X/m-p/1426836#M14380</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-03-11T10:35:37Z</dc:date>
    </item>
  </channel>
</rss>