<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [S32K144] Binary file in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-Binary-file/m-p/1419542#M14159</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32K144.&lt;BR /&gt;I want to read a binary file, but when I try to read the file with the fopen function, it returns NULL.&lt;BR /&gt;Is it possible to read binary files with S32K144? If so, could you please give me an example?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;KK2&lt;/P&gt;</description>
    <pubDate>Fri, 25 Feb 2022 05:58:16 GMT</pubDate>
    <dc:creator>KK2</dc:creator>
    <dc:date>2022-02-25T05:58:16Z</dc:date>
    <item>
      <title>[S32K144] Binary file</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Binary-file/m-p/1419542#M14159</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32K144.&lt;BR /&gt;I want to read a binary file, but when I try to read the file with the fopen function, it returns NULL.&lt;BR /&gt;Is it possible to read binary files with S32K144? If so, could you please give me an example?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;KK2&lt;/P&gt;</description>
      <pubDate>Fri, 25 Feb 2022 05:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Binary-file/m-p/1419542#M14159</guid>
      <dc:creator>KK2</dc:creator>
      <dc:date>2022-02-25T05:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K144] Binary file</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-Binary-file/m-p/1419746#M14171</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;it would be necessary to implement file system. Otherwise the fopen cannot be used. We do not have such example.&lt;/P&gt;
&lt;P&gt;Not sure what is your goal but common way is to link a bin file to your project as described here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Link-a-binary-file-s-into-the-application-project-using/ta-p/1111536" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Link-a-binary-file-s-into-the-application-project-using/ta-p/1111536&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;And then you can access the bin file directly without fopen function and without file system.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 25 Feb 2022 10:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-Binary-file/m-p/1419746#M14171</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-02-25T10:40:58Z</dc:date>
    </item>
  </channel>
</rss>