<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックProgramming conditions</title>
    <link>https://community.nxp.com/t5/S32K/Programming-conditions/m-p/1419091#M14141</link>
    <description>&lt;P&gt;We are developping a Bootloader for the NXP S32K118. Is there any condition we need to check before reprogramming the Flash memory? For example:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there any voltage range of the microcontroller (VDD) where it is not secure/recommended to reprogramm flash?&lt;/LI&gt;&lt;LI&gt;Is there any temperature range at the microcontroller where it is not secure/recommended to reprogramm flash?&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Thu, 24 Feb 2022 12:39:48 GMT</pubDate>
    <dc:creator>MMT_BW</dc:creator>
    <dc:date>2022-02-24T12:39:48Z</dc:date>
    <item>
      <title>Programming conditions</title>
      <link>https://community.nxp.com/t5/S32K/Programming-conditions/m-p/1419091#M14141</link>
      <description>&lt;P&gt;We are developping a Bootloader for the NXP S32K118. Is there any condition we need to check before reprogramming the Flash memory? For example:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there any voltage range of the microcontroller (VDD) where it is not secure/recommended to reprogramm flash?&lt;/LI&gt;&lt;LI&gt;Is there any temperature range at the microcontroller where it is not secure/recommended to reprogramm flash?&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Thu, 24 Feb 2022 12:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Programming-conditions/m-p/1419091#M14141</guid>
      <dc:creator>MMT_BW</dc:creator>
      <dc:date>2022-02-24T12:39:48Z</dc:date>
    </item>
    <item>
      <title>Re: Programming conditions</title>
      <link>https://community.nxp.com/t5/S32K/Programming-conditions/m-p/1419708#M14166</link>
      <description>&lt;P&gt;Hi Melissa,&lt;BR /&gt;Flash operations are supported across whole functional temperature and voltage range. &lt;BR /&gt;In case of S32K14x, CSEc and EEPROM writes/erase cannot be executed in high speed run mode (HSRUN). But that’s not an issue in case of S32K118 because it does not support HSRUN.&lt;BR /&gt;So, the only thing I can see is to check if some operation is already running:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1645782127423.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171782iED54D7AB1D4E5889/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1645782127423.png" alt="lukaszadrapa_0-1645782127423.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1645782127423.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you use SDK/RTD, it’s checked by drivers. But short time ago I reported possible issue because CSEc SDK drivers do not check if flash operation is running. This is not fixed yet. Current workaround is to check this by yourself. &lt;BR /&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 25 Feb 2022 09:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Programming-conditions/m-p/1419708#M14166</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-02-25T09:43:53Z</dc:date>
    </item>
  </channel>
</rss>