<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: VLPS &amp;LPIT &amp; CAN</title>
    <link>https://community.nxp.com/t5/S32K/VLPS-LPIT-CAN/m-p/706176#M1403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As you can see in Chapter 53.13 Debug in low-power modes, with debug enabled, transitions from Run directly to VLPS are not allowed and result in the system entering Stop mode instead.&lt;/P&gt;&lt;P&gt;So, in this case, it seems the LPIT wake up from VLPS.&lt;/P&gt;&lt;P&gt;But in stand-alone mode the LPIT as well as CAN cannot wake up from VLPS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Aug 2017 14:49:24 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-08-29T14:49:24Z</dc:date>
    <item>
      <title>VLPS &amp;LPIT &amp; CAN</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-LPIT-CAN/m-p/706175#M1402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;What is the difference between debug and run mode? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why does lpit wake up s32k144 running in VLPs mode in debug mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P dir="ltr" style="display: none;"&gt;为什么仅仅初始化了CAN模块，CAN可以唤醒S32K在VLPS模式？&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why CAN can wake up S32K in VLPS mode，just initialize the CAN module ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thank you very much&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 05:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-LPIT-CAN/m-p/706175#M1402</guid>
      <dc:creator>panda_fei</dc:creator>
      <dc:date>2017-08-24T05:30:14Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS &amp;LPIT &amp; CAN</title>
      <link>https://community.nxp.com/t5/S32K/VLPS-LPIT-CAN/m-p/706176#M1403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As you can see in Chapter 53.13 Debug in low-power modes, with debug enabled, transitions from Run directly to VLPS are not allowed and result in the system entering Stop mode instead.&lt;/P&gt;&lt;P&gt;So, in this case, it seems the LPIT wake up from VLPS.&lt;/P&gt;&lt;P&gt;But in stand-alone mode the LPIT as well as CAN cannot wake up from VLPS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 14:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/VLPS-LPIT-CAN/m-p/706176#M1403</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-08-29T14:49:24Z</dc:date>
    </item>
  </channel>
</rss>