<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックERM module question</title>
    <link>https://community.nxp.com/t5/S32K/ERM-module-question/m-p/1412775#M13974</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I see sample ERM and EIM，I am not very clear about the relationship between these two modules.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Is this EIM module used to detect that the ERM module is in effect? I mean&amp;nbsp; when I use ERM module, I need to use EIM module to detect ERM module is running. so the EIM module just use to detect the ERM module if running?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Feb 2022 01:59:16 GMT</pubDate>
    <dc:creator>asd046012</dc:creator>
    <dc:date>2022-02-14T01:59:16Z</dc:date>
    <item>
      <title>ERM module question</title>
      <link>https://community.nxp.com/t5/S32K/ERM-module-question/m-p/1412775#M13974</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I see sample ERM and EIM，I am not very clear about the relationship between these two modules.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Is this EIM module used to detect that the ERM module is in effect? I mean&amp;nbsp; when I use ERM module, I need to use EIM module to detect ERM module is running. so the EIM module just use to detect the ERM module if running?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 01:59:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ERM-module-question/m-p/1412775#M13974</guid>
      <dc:creator>asd046012</dc:creator>
      <dc:date>2022-02-14T01:59:16Z</dc:date>
    </item>
    <item>
      <title>Re: ERM module question</title>
      <link>https://community.nxp.com/t5/S32K/ERM-module-question/m-p/1412854#M13978</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@asd046012" target="_blank"&gt;Hi@asd046012&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;please taka a look at the &lt;STRONG&gt;S32K-RM&amp;nbsp;&lt;/STRONG&gt;for more infos.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Chapter 21 : Error Injection Module(EIM)&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The EIM(Error Injection module) is mainly usef for diagonstic purposes.It provides a method for diagnostic coverage of the peripheral memories.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Chapter 22:Error Reporting Module(ERM)&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The Error Reporting Module (ERM) provides information and optional interrupt&lt;BR /&gt;notification on memory error events associated with Error Correction Code (ECC).&lt;/P&gt;
&lt;P&gt;简单点说就是，一般情况下ECC不会出错，这时你不好验证你处理ECC的流程是否真确，这个时候你可以用EIM去注入一个ECC错误，然后验证你处理ECC错误的流程是否正确。如果验证完你ECC错误处理的流程没啥问题，在量产产品中，你完全可以去掉EIM模块。&lt;/P&gt;
&lt;P&gt;关于ECC错误流程发生后的处理，你可以参考：&lt;STRONG&gt;AN12522 S32K1xx ECC Error Handling&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Jim,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 05:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ERM-module-question/m-p/1412854#M13978</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2022-02-14T05:33:17Z</dc:date>
    </item>
  </channel>
</rss>