<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144 interface voltage for ISELED in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1411877#M13946</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the S32K144 is connected to iseledstrip through an adapter board.&lt;/P&gt;&lt;P&gt;The voltage from MCU is 3.3V while LED strip requires 5V. Could the MCU be damaged during read function?&lt;/P&gt;&lt;P&gt;See ISELED ADK User Manual.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Neo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Feb 2022 14:37:54 GMT</pubDate>
    <dc:creator>nanjun</dc:creator>
    <dc:date>2022-02-10T14:37:54Z</dc:date>
    <item>
      <title>S32K144 interface voltage for ISELED</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1411877#M13946</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;the S32K144 is connected to iseledstrip through an adapter board.&lt;/P&gt;&lt;P&gt;The voltage from MCU is 3.3V while LED strip requires 5V. Could the MCU be damaged during read function?&lt;/P&gt;&lt;P&gt;See ISELED ADK User Manual.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Neo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Feb 2022 14:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1411877#M13946</guid>
      <dc:creator>nanjun</dc:creator>
      <dc:date>2022-02-10T14:37:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 interface voltage for ISELED</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1412385#M13959</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;when the supply voltage is 3.3V, the MCU is not 5V tolerant even if a pin is configured as open drain. The datasheet explicitly states that open drain pin must be pulled to VDD. And Vih spec says that input voltage can't exceed VDD+0.3V. If an external circuit requires 5V, the only options are either to use 5V supply voltage for MCU or use some voltage level translator.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 11 Feb 2022 10:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1412385#M13959</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-02-11T10:05:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 interface voltage for ISELED</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1416325#M14060</link>
      <description>&lt;P&gt;Hello Lucas,&lt;/P&gt;&lt;P&gt;thanks for your reply. Actualley I wrote you back some days before but it seems the email failed.&lt;/P&gt;&lt;P&gt;The problem was solved.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Neo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Feb 2022 18:42:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-interface-voltage-for-ISELED/m-p/1416325#M14060</guid>
      <dc:creator>nanjun</dc:creator>
      <dc:date>2022-02-20T18:42:39Z</dc:date>
    </item>
  </channel>
</rss>