<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I setup communication between SAMV71 MCU and  MC33771B through SPI? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-do-I-setup-communication-between-SAMV71-MCU-and-MC33771B/m-p/1408513#M13874</link>
    <description>&lt;P&gt;I am currently trying to use FRDM33771BSPIEV to monitor 8 cell voltages. I have connected the hardware&lt;/P&gt;&lt;P&gt;according to the user manual and the 4 wire SPI connections have also been setup. Here SAMV71 is master and MC33771B is slave module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)How do I receive messages from MC33771B?&lt;/P&gt;&lt;P&gt;2)How do I program MC33771B i.e what instructions do I use?(some commands such as MEAS_STACK have been mentioned in the data sheet, do I use them?)&lt;/P&gt;&lt;P&gt;3) Are there any examples files to control MC33771B or to atleast retrieve data from MC33771B?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Feb 2022 10:17:13 GMT</pubDate>
    <dc:creator>MuraliKK</dc:creator>
    <dc:date>2022-02-03T10:17:13Z</dc:date>
    <item>
      <title>How do I setup communication between SAMV71 MCU and  MC33771B through SPI?</title>
      <link>https://community.nxp.com/t5/S32K/How-do-I-setup-communication-between-SAMV71-MCU-and-MC33771B/m-p/1408513#M13874</link>
      <description>&lt;P&gt;I am currently trying to use FRDM33771BSPIEV to monitor 8 cell voltages. I have connected the hardware&lt;/P&gt;&lt;P&gt;according to the user manual and the 4 wire SPI connections have also been setup. Here SAMV71 is master and MC33771B is slave module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)How do I receive messages from MC33771B?&lt;/P&gt;&lt;P&gt;2)How do I program MC33771B i.e what instructions do I use?(some commands such as MEAS_STACK have been mentioned in the data sheet, do I use them?)&lt;/P&gt;&lt;P&gt;3) Are there any examples files to control MC33771B or to atleast retrieve data from MC33771B?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 10:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-do-I-setup-communication-between-SAMV71-MCU-and-MC33771B/m-p/1408513#M13874</guid>
      <dc:creator>MuraliKK</dc:creator>
      <dc:date>2022-02-03T10:17:13Z</dc:date>
    </item>
    <item>
      <title>Re: How do I setup communication between SAMV71 MCU and  MC33771B through SPI?</title>
      <link>https://community.nxp.com/t5/S32K/How-do-I-setup-communication-between-SAMV71-MCU-and-MC33771B/m-p/1408610#M13881</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;we provide this SW package which includes generic driver suitable for any 32bit MCU with SPI module and example for S32K144 MCU:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/analog-expert-software-and-tools/sdk-analog-expert-drivers/embedded-sw-battery-cell-controller-software-driver-for-mc33771b-mc33772b:EMBEDDED-SW-BCC" target="_blank"&gt;https://www.nxp.com/design/analog-expert-software-and-tools/sdk-analog-expert-drivers/embedded-sw-battery-cell-controller-software-driver-for-mc33771b-mc33772b:EMBEDDED-SW-BCC&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 13:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-do-I-setup-communication-between-SAMV71-MCU-and-MC33771B/m-p/1408610#M13881</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2022-02-03T13:15:21Z</dc:date>
    </item>
  </channel>
</rss>