<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unused pin configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705443#M1385</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please refer to &lt;A href="http://www.nxp.com/docs/en/application-note/AN5426.pdf"&gt;AN542 Hardware Design Guidelines for S32K1xx Microcontrollers&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;See Chapter 8 Unused pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 21:23:40 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-08-23T21:23:40Z</dc:date>
    <item>
      <title>Unused pin configuration</title>
      <link>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705442#M1384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;My target is S32k144 and we're required to&amp;nbsp;place the part&amp;nbsp;in&amp;nbsp;one of the low power mode (have not decided which one yet) and therefore need to know which is the best way to configure the unused pin&amp;nbsp;to prevent any unwanted current consumption through high input impedance CMOS&amp;nbsp;pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there is a recommendation to:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Pull all unused analog pins low via an external resistor.&lt;/LI&gt;&lt;LI&gt;leave all the digital unused pins in their default state(inactive)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Is this correct?&lt;/P&gt;&lt;P&gt;Not sure what inactive state is? are they floating ? if yes they should not be configured as such.&lt;/P&gt;&lt;P&gt;Please educated me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 17:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705442#M1384</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2017-08-23T17:53:44Z</dc:date>
    </item>
    <item>
      <title>Re: Unused pin configuration</title>
      <link>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705443#M1385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please refer to &lt;A href="http://www.nxp.com/docs/en/application-note/AN5426.pdf"&gt;AN542 Hardware Design Guidelines for S32K1xx Microcontrollers&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;See Chapter 8 Unused pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 21:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705443#M1385</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-08-23T21:23:40Z</dc:date>
    </item>
    <item>
      <title>Re: Unused pin configuration</title>
      <link>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705444#M1386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for you response，it is a useful message for me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Aug 2017 05:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unused-pin-configuration/m-p/705444#M1386</guid>
      <dc:creator>jinshuaixu</dc:creator>
      <dc:date>2017-08-24T05:10:54Z</dc:date>
    </item>
  </channel>
</rss>