<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k144 : Difference betweend UID in CSE and Unique Identification Register in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404457#M13788</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;These two number are absolutely different and not connected each other.&lt;/P&gt;
&lt;P&gt;UID stored in the identification register (laded from IFR during reset) is an unique number of the MCU and can be read from the register anytime as from any register.&lt;/P&gt;
&lt;P&gt;UID in CSE is connected to the SHE Functional Specification and can be read only by GET_ID command.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jan 2022 09:00:24 GMT</pubDate>
    <dc:creator>lama</dc:creator>
    <dc:date>2022-01-25T09:00:24Z</dc:date>
    <item>
      <title>s32k144 : Difference betweend UID in CSE and Unique Identification Register</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404299#M13784</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need certain value that is never the same with the other.&lt;/P&gt;&lt;P&gt;(I guess this value is called UID in general)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Common thing : 1. Both of them are 16 byte.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 2. The value depends on chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;what's difference?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And every s32k144 chip has their own distinct value on the world?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 04:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404299#M13784</guid>
      <dc:creator>kmh48301</dc:creator>
      <dc:date>2022-01-25T04:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 : Difference betweend UID in CSE and Unique Identification Register</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404457#M13788</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;These two number are absolutely different and not connected each other.&lt;/P&gt;
&lt;P&gt;UID stored in the identification register (laded from IFR during reset) is an unique number of the MCU and can be read from the register anytime as from any register.&lt;/P&gt;
&lt;P&gt;UID in CSE is connected to the SHE Functional Specification and can be read only by GET_ID command.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jan 2022 09:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404457#M13788</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-01-25T09:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 : Difference betweend UID in CSE and Unique Identification Register</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404830#M13796</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does NXP ensure that&amp;nbsp;the 'uid' value written in the 'Unique Identification Register'&lt;/P&gt;&lt;P&gt;of every chip is different?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please explain me detail&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Phillip&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jan 2022 00:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1404830#M13796</guid>
      <dc:creator>kmh48301</dc:creator>
      <dc:date>2022-01-26T00:36:15Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 : Difference betweend UID in CSE and Unique Identification Register</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1407007#M13847</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The UID is loaded into IFR during manufacturing process and it is set for each device as identifier of the device and placed into our internal records about device. I am not able to say more.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Mon, 31 Jan 2022 10:16:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-Difference-betweend-UID-in-CSE-and-Unique-Identification/m-p/1407007#M13847</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2022-01-31T10:16:26Z</dc:date>
    </item>
  </channel>
</rss>