<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Get SDID value for S32K118EVB in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Get-SDID-value-for-S32K118EVB/m-p/1398247#M13627</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32K118EVB and need to get SDID details. I found the below lines of code in the project i am using:&lt;/P&gt;&lt;P&gt;/* SDID Bit Fields */&lt;BR /&gt;#define SIM_SDID_FEATURES_MASK 0xFFu&lt;BR /&gt;#define SIM_SDID_FEATURES_SHIFT 0u&lt;BR /&gt;#define SIM_SDID_FEATURES_WIDTH 8u&lt;BR /&gt;#define SIM_SDID_FEATURES(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_FEATURES_SHIFT))&amp;amp;SIM_SDID_FEATURES_MASK)&lt;BR /&gt;#define SIM_SDID_PACKAGE_MASK 0xF00u&lt;BR /&gt;#define SIM_SDID_PACKAGE_SHIFT 8u&lt;BR /&gt;#define SIM_SDID_PACKAGE_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_PACKAGE(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_PACKAGE_SHIFT))&amp;amp;SIM_SDID_PACKAGE_MASK)&lt;BR /&gt;#define SIM_SDID_REVID_MASK 0xF000u&lt;BR /&gt;#define SIM_SDID_REVID_SHIFT 12u&lt;BR /&gt;#define SIM_SDID_REVID_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_REVID(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_REVID_SHIFT))&amp;amp;SIM_SDID_REVID_MASK)&lt;BR /&gt;#define SIM_SDID_RAMSIZE_MASK 0xF0000u&lt;BR /&gt;#define SIM_SDID_RAMSIZE_SHIFT 16u&lt;BR /&gt;#define SIM_SDID_RAMSIZE_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_RAMSIZE(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_RAMSIZE_SHIFT))&amp;amp;SIM_SDID_RAMSIZE_MASK)&lt;BR /&gt;#define SIM_SDID_DERIVATE_MASK 0xF00000u&lt;BR /&gt;#define SIM_SDID_DERIVATE_SHIFT 20u&lt;BR /&gt;#define SIM_SDID_DERIVATE_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_DERIVATE(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_DERIVATE_SHIFT))&amp;amp;SIM_SDID_DERIVATE_MASK)&lt;BR /&gt;#define SIM_SDID_SUBSERIES_MASK 0xF000000u&lt;BR /&gt;#define SIM_SDID_SUBSERIES_SHIFT 24u&lt;BR /&gt;#define SIM_SDID_SUBSERIES_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_SUBSERIES(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_SUBSERIES_SHIFT))&amp;amp;SIM_SDID_SUBSERIES_MASK)&lt;BR /&gt;#define SIM_SDID_GENERATION_MASK 0xF0000000u&lt;BR /&gt;#define SIM_SDID_GENERATION_SHIFT 28u&lt;BR /&gt;#define SIM_SDID_GENERATION_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_GENERATION(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_GENERATION_SHIFT))&amp;amp;SIM_SDID_GENERATION_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I use these functions to get the version details? Could you please suggest which one to use and what needs to be passed as the argument 'x'?&lt;/P&gt;&lt;P&gt;I need the details so that I can transmit the same serially for the project our team is working on.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jan 2022 16:47:52 GMT</pubDate>
    <dc:creator>rahulpkumar-2612</dc:creator>
    <dc:date>2022-01-12T16:47:52Z</dc:date>
    <item>
      <title>Get SDID value for S32K118EVB</title>
      <link>https://community.nxp.com/t5/S32K/Get-SDID-value-for-S32K118EVB/m-p/1398247#M13627</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using S32K118EVB and need to get SDID details. I found the below lines of code in the project i am using:&lt;/P&gt;&lt;P&gt;/* SDID Bit Fields */&lt;BR /&gt;#define SIM_SDID_FEATURES_MASK 0xFFu&lt;BR /&gt;#define SIM_SDID_FEATURES_SHIFT 0u&lt;BR /&gt;#define SIM_SDID_FEATURES_WIDTH 8u&lt;BR /&gt;#define SIM_SDID_FEATURES(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_FEATURES_SHIFT))&amp;amp;SIM_SDID_FEATURES_MASK)&lt;BR /&gt;#define SIM_SDID_PACKAGE_MASK 0xF00u&lt;BR /&gt;#define SIM_SDID_PACKAGE_SHIFT 8u&lt;BR /&gt;#define SIM_SDID_PACKAGE_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_PACKAGE(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_PACKAGE_SHIFT))&amp;amp;SIM_SDID_PACKAGE_MASK)&lt;BR /&gt;#define SIM_SDID_REVID_MASK 0xF000u&lt;BR /&gt;#define SIM_SDID_REVID_SHIFT 12u&lt;BR /&gt;#define SIM_SDID_REVID_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_REVID(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_REVID_SHIFT))&amp;amp;SIM_SDID_REVID_MASK)&lt;BR /&gt;#define SIM_SDID_RAMSIZE_MASK 0xF0000u&lt;BR /&gt;#define SIM_SDID_RAMSIZE_SHIFT 16u&lt;BR /&gt;#define SIM_SDID_RAMSIZE_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_RAMSIZE(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_RAMSIZE_SHIFT))&amp;amp;SIM_SDID_RAMSIZE_MASK)&lt;BR /&gt;#define SIM_SDID_DERIVATE_MASK 0xF00000u&lt;BR /&gt;#define SIM_SDID_DERIVATE_SHIFT 20u&lt;BR /&gt;#define SIM_SDID_DERIVATE_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_DERIVATE(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_DERIVATE_SHIFT))&amp;amp;SIM_SDID_DERIVATE_MASK)&lt;BR /&gt;#define SIM_SDID_SUBSERIES_MASK 0xF000000u&lt;BR /&gt;#define SIM_SDID_SUBSERIES_SHIFT 24u&lt;BR /&gt;#define SIM_SDID_SUBSERIES_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_SUBSERIES(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_SUBSERIES_SHIFT))&amp;amp;SIM_SDID_SUBSERIES_MASK)&lt;BR /&gt;#define SIM_SDID_GENERATION_MASK 0xF0000000u&lt;BR /&gt;#define SIM_SDID_GENERATION_SHIFT 28u&lt;BR /&gt;#define SIM_SDID_GENERATION_WIDTH 4u&lt;BR /&gt;#define SIM_SDID_GENERATION(x) (((uint32_t)(((uint32_t)(x))&amp;lt;&amp;lt;SIM_SDID_GENERATION_SHIFT))&amp;amp;SIM_SDID_GENERATION_MASK)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I use these functions to get the version details? Could you please suggest which one to use and what needs to be passed as the argument 'x'?&lt;/P&gt;&lt;P&gt;I need the details so that I can transmit the same serially for the project our team is working on.&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 16:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Get-SDID-value-for-S32K118EVB/m-p/1398247#M13627</guid>
      <dc:creator>rahulpkumar-2612</dc:creator>
      <dc:date>2022-01-12T16:47:52Z</dc:date>
    </item>
    <item>
      <title>Re: Get SDID value for S32K118EVB</title>
      <link>https://community.nxp.com/t5/S32K/Get-SDID-value-for-S32K118EVB/m-p/1398452#M13630</link>
      <description>&lt;P&gt;Hi&amp;nbsp;rahulpkumar,&lt;/P&gt;
&lt;P&gt;Please read the&amp;nbsp;&lt;A id="relatedDocsClick_1" href="https://www.nxp.com/webapp/Download?colCode=S32K1XXRM" target="_blank" rel="noopener"&gt;&lt;STRONG&gt;S32K1xx MCU Family - Reference Manual&lt;/STRONG&gt;&lt;/A&gt;&amp;nbsp;for more detail about SDID:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="11.3.1.8 System Device Identification Register (SDID).png" style="width: 504px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167464iBD1E930CE6228FC1/image-size/large?v=v2&amp;amp;px=999" role="button" title="11.3.1.8 System Device Identification Register (SDID).png" alt="11.3.1.8 System Device Identification Register (SDID).png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="11.3.1.8 System Device Identification Register (SDID) FEATURES.png" style="width: 777px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/167465iC7E583AEE8B9006E/image-size/large?v=v2&amp;amp;px=999" role="button" title="11.3.1.8 System Device Identification Register (SDID) FEATURES.png" alt="11.3.1.8 System Device Identification Register (SDID) FEATURES.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 00:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Get-SDID-value-for-S32K118EVB/m-p/1398452#M13630</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-01-13T00:34:19Z</dc:date>
    </item>
  </channel>
</rss>