<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: CAN message IDX</title>
    <link>https://community.nxp.com/t5/S32K/CAN-message-IDX/m-p/1395049#M13546</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;mb_idx specifies index of used message buffer (MB). On S32K148 each FlexCAN module includes 32 MBs (assuming 8 byte payload), indexed from 0 to 31, and each MB can be configured to transmit or receive CAN message.&lt;BR /&gt;More info can be found in FlexCAN chapter of the device Reference Manual.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 05 Jan 2022 20:27:50 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-01-05T20:27:50Z</dc:date>
    <item>
      <title>CAN message IDX</title>
      <link>https://community.nxp.com/t5/S32K/CAN-message-IDX/m-p/1394936#M13545</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I use the S32K148EVB to send CAN.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It works correctly but I don't know what "uint8_t mb_idx" is.&lt;/P&gt;&lt;P&gt;I did not find any information in the S32K-RM.&lt;/P&gt;&lt;P&gt;Is it related to the CAN functionality? Or the S32k CAN driver? Is there an explanation?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 16:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-message-IDX/m-p/1394936#M13545</guid>
      <dc:creator>Milado</dc:creator>
      <dc:date>2022-01-05T16:12:01Z</dc:date>
    </item>
    <item>
      <title>Re: CAN message IDX</title>
      <link>https://community.nxp.com/t5/S32K/CAN-message-IDX/m-p/1395049#M13546</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;mb_idx specifies index of used message buffer (MB). On S32K148 each FlexCAN module includes 32 MBs (assuming 8 byte payload), indexed from 0 to 31, and each MB can be configured to transmit or receive CAN message.&lt;BR /&gt;More info can be found in FlexCAN chapter of the device Reference Manual.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jan 2022 20:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-message-IDX/m-p/1395049#M13546</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-01-05T20:27:50Z</dc:date>
    </item>
  </channel>
</rss>