<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: CAN FD  Error  in S32k144</title>
    <link>https://community.nxp.com/t5/S32K/CAN-FD-Error-in-S32k144/m-p/1393802#M13493</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;be sure board is powered by 12V and SBC's transceiver is active. Is there anything transmitted by S32K144? Is there any error detected (check ESR1 ECR registers)?&lt;BR /&gt;check if both nodes uses same CAN bit timing (arbitration/data phases, sample points) and same protocol is used (ISO FD, non-ISO FD)&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 03 Jan 2022 15:16:10 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-01-03T15:16:10Z</dc:date>
    <item>
      <title>CAN FD  Error  in S32k144</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-Error-in-S32k144/m-p/1393595#M13480</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I&amp;nbsp;&lt;/SPAN&gt;am using the S32k144 evaluation board and I am trying to establish CAN FD communication between it and the Canoe environment.&lt;/P&gt;&lt;P&gt;I configured S32k144 with arbitration phase bit rate 500kb/s and data phase bit rate 2Mb/s&lt;/P&gt;&lt;P&gt;When I start canoe with real bus, it gives me not acknowledge error:&lt;/P&gt;&lt;P&gt;But while I am trying to connect through IG block and simulation bus it's working as expected.&lt;/P&gt;&lt;P&gt;Could you please suggest ..what is the exact issue and solution for this issue?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pratyay&lt;/P&gt;</description>
      <pubDate>Sat, 01 Jan 2022 19:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-Error-in-S32k144/m-p/1393595#M13480</guid>
      <dc:creator>pratayay123</dc:creator>
      <dc:date>2022-01-01T19:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: CAN FD  Error  in S32k144</title>
      <link>https://community.nxp.com/t5/S32K/CAN-FD-Error-in-S32k144/m-p/1393802#M13493</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;be sure board is powered by 12V and SBC's transceiver is active. Is there anything transmitted by S32K144? Is there any error detected (check ESR1 ECR registers)?&lt;BR /&gt;check if both nodes uses same CAN bit timing (arbitration/data phases, sample points) and same protocol is used (ISO FD, non-ISO FD)&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jan 2022 15:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-FD-Error-in-S32k144/m-p/1393802#M13493</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-01-03T15:16:10Z</dc:date>
    </item>
  </channel>
</rss>