<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Importing a Memory Dump File Error in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1393015#M13461</link>
    <description>&lt;P&gt;Thank you Daniel for the comment !&lt;/P&gt;</description>
    <pubDate>Wed, 29 Dec 2021 10:06:49 GMT</pubDate>
    <dc:creator>turgaykale</dc:creator>
    <dc:date>2021-12-29T10:06:49Z</dc:date>
    <item>
      <title>Error For Importing a Memory Dump File to FlexNVM EERAM</title>
      <link>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1391839#M13390</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using an EEPROM Emulation feature of FlexNVM in S32K148 MCU. I am using S32 Design Studio v3.4 IDE. I have got an error when importing a memory dump file (already exported and saved in srec format) to FlexRAM address starting from 0x1400_0000 to 0x1400_0400 which is a FlexRAM memory range used to emulate EEPROM Emulation feature of FlexNVM. Would you please help to understand the reason behind this type of error? Is it possible to import a memory dump file to FlexRAM (in our case: address from 0x1400_0000 to 0x1400_0400) when using an EEPROM emulation feature of FlexNVM ?&lt;/P&gt;&lt;P&gt;Importing a memory dump file (srec format) via memory browser window:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="turgaykale_1-1640348317902.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166211i7FD23EBFDEBC7FA5/image-size/large?v=v2&amp;amp;px=999" role="button" title="turgaykale_1-1640348317902.png" alt="turgaykale_1-1640348317902.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;turgaykale_1-1640348317902.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Error is:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="turgaykale_2-1640348673247.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/166212i3294BD9EECF72CE2/image-size/large?v=v2&amp;amp;px=999" role="button" title="turgaykale_2-1640348673247.png" alt="turgaykale_2-1640348673247.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;turgaykale_2-1640348673247.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Dec 2021 10:18:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1391839#M13390</guid>
      <dc:creator>turgaykale</dc:creator>
      <dc:date>2021-12-29T10:18:21Z</dc:date>
    </item>
    <item>
      <title>Re: Importing a Memory Dump File Error</title>
      <link>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1392634#M13443</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194080"&gt;@turgaykale&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;When EEERDY = 1, every write (8bit, 16bit or 32bit) to the EEEPROM clears the CCIF flag and the EEPROM must not be written until CCIF is set again.&lt;/P&gt;
&lt;P&gt;Please refer to AN11983 Using the S32K1xx EEPROM Functionality&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11983.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on that, I don't think the S32DS can do that.&lt;/P&gt;
&lt;P&gt;It should be possible to load the data to SRAM.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 28 Dec 2021 09:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1392634#M13443</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-28T09:53:36Z</dc:date>
    </item>
    <item>
      <title>Re: Importing a Memory Dump File Error</title>
      <link>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1393015#M13461</link>
      <description>&lt;P&gt;Thank you Daniel for the comment !&lt;/P&gt;</description>
      <pubDate>Wed, 29 Dec 2021 10:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Error-For-Importing-a-Memory-Dump-File-to-FlexNVM-EERAM/m-p/1393015#M13461</guid>
      <dc:creator>turgaykale</dc:creator>
      <dc:date>2021-12-29T10:06:49Z</dc:date>
    </item>
  </channel>
</rss>