<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックIs there any position independent code example for S32K148?</title>
    <link>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1391840#M13391</link>
    <description>&lt;P&gt;I want to generate position independent code image(SREC file) for S32K148. I have tried to modify hello_world example; but I could not generate successfully. Is there any example project and could you please share it if it is avaible?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Dec 2021 12:39:12 GMT</pubDate>
    <dc:creator>hkaracali</dc:creator>
    <dc:date>2021-12-24T12:39:12Z</dc:date>
    <item>
      <title>Is there any position independent code example for S32K148?</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1391840#M13391</link>
      <description>&lt;P&gt;I want to generate position independent code image(SREC file) for S32K148. I have tried to modify hello_world example; but I could not generate successfully. Is there any example project and could you please share it if it is avaible?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Dec 2021 12:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1391840#M13391</guid>
      <dc:creator>hkaracali</dc:creator>
      <dc:date>2021-12-24T12:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any position independent code example for S32K148?</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392122#M13404</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@hkaracali" target="_blank"&gt;Hi@hkaracali&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Do you want to modeified LD file or something else? I send you an App demo privately which used for an Bootloader example,I don't know if it is what you want.&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Jim,&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 07:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392122#M13404</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-12-27T07:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any position independent code example for S32K148?</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392132#M13406</link>
      <description>&lt;P&gt;Hi Jim,&lt;/P&gt;&lt;P&gt;I am looking for an example_app which generates position independent code(PIC). Because I have develop a bootloader. I can flash my app into the flash memory according to its linker file and it runs successfully. Every thing is OK up to now. However I want to move my app to different sector on flash memory. If I do that my app does not run anymore normally. So I want to generate PIC app which can be run from anywhere on the flash. Therefore I asked an example app like this.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 07:13:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392132#M13406</guid>
      <dc:creator>hkaracali</dc:creator>
      <dc:date>2021-12-27T07:13:13Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any position independent code example for S32K148?</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392156#M13413</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@hkaracali" target="_blank"&gt;Hi@hkaracali&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;try to refer to this link below.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/EXAMPLE-S32K144-Position-Independent-Code/ta-p/1102520" target="_self"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/EXAMPLE-S32K144-Position-Independent-Code/ta-p/1102520&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 07:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392156#M13413</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-12-27T07:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any position independent code example for S32K148?</title>
      <link>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392183#M13417</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I had a look it before. I have tried to apply mentioned updates to S32K148; but it did not works successfully. So, I am looking for an example now.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Dec 2021 08:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-there-any-position-independent-code-example-for-S32K148/m-p/1392183#M13417</guid>
      <dc:creator>hkaracali</dc:creator>
      <dc:date>2021-12-27T08:42:26Z</dc:date>
    </item>
  </channel>
</rss>