<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 ADC in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701136#M1339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Thanks for reply. That means if I want to use more than 8 channel in back to back mode then I can use ADC0&amp;nbsp; eight channels and ADC1 eight channels ( I tested it is working fine) . In single ADC module I can't use more than 8 channels. Is it correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ravi Ranjan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Oct 2017 09:36:05 GMT</pubDate>
    <dc:creator>raviranjankumar</dc:creator>
    <dc:date>2017-10-11T09:36:05Z</dc:date>
    <item>
      <title>S32K144 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701134#M1337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am working on S32K144 EVB. I want to configure more than 8 channel at a time. I am using PDB trigger in back to back mode. Up to 9 channel it is working fine. but after that I am not getting result. I am configuring PDB0 channel0 for first 8 channel and PDB0 channel1 for next 8 channel. To trigger&amp;nbsp; first 8 channel I am giving CH0C1.EN = FF,&amp;nbsp;&lt;/P&gt;&lt;P&gt;CH0C1.BB = FE (PDB0 channel0) and same for PDB0 channel1 to configure next 8 channel. Is it correct ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My configurations are ADC_ALTCLK1, 12-Bit Mode, Divide ratio is 4, sample time is 12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help me. waiting for response....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regard&lt;/P&gt;&lt;P&gt;Ravi Ranjan Kumar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Oct 2017 14:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701134#M1337</guid>
      <dc:creator>raviranjankumar</dc:creator>
      <dc:date>2017-10-07T14:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701135#M1338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ravi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the PDB0 ch0 to PDB0 ch1 back-to-back chaining is not possible. PDB back to back operation forming a ring is supported only on Channel 0 and so just PDB0-PDB1 ring is possible if SIM_CHIPCTL[PDB_BB_SEL]=1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/14509iA4E53DBC478EFC86/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 07:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701135#M1338</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-10-11T07:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701136#M1339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Thanks for reply. That means if I want to use more than 8 channel in back to back mode then I can use ADC0&amp;nbsp; eight channels and ADC1 eight channels ( I tested it is working fine) . In single ADC module I can't use more than 8 channels. Is it correct?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Ravi Ranjan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 09:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701136#M1339</guid>
      <dc:creator>raviranjankumar</dc:creator>
      <dc:date>2017-10-11T09:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701137#M1340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ravi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, the back-to-back connection between channels within PDB module is not available. Tables 41-4/41-5 gives you a summary.&lt;/P&gt;&lt;P&gt;If you want to use more than 8 channels on single ADC module then you need to trigger each PDB0 channels separately with proper delay, so the chain is finished before next is started.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 10:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701137#M1340</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-10-11T10:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701138#M1341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Petr,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; Thank you so much. It was really helpful for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ravi Ranjan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 12:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701138#M1341</guid>
      <dc:creator>raviranjankumar</dc:creator>
      <dc:date>2017-10-11T12:09:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ADC</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701139#M1342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ravi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;Did you configure it successfully? And can you share your code for me? I can not configure it successfully.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 12:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ADC/m-p/701139#M1342</guid>
      <dc:creator>frankzeng</dc:creator>
      <dc:date>2018-03-09T12:09:04Z</dc:date>
    </item>
  </channel>
</rss>