<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックSimulate I2S on S32K144</title>
    <link>https://community.nxp.com/t5/S32K/Simulate-I2S-on-S32K144/m-p/700890#M1332</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to setup a system which supports 2 channel input and 6 channel output on S32K144.&lt;/P&gt;&lt;P&gt;There was an example in SDK, but it only has 2 Channel input and 2 Channel output.&lt;/P&gt;&lt;P&gt;My system will look like:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;FlexIO pins configured as SCK, WS, IN1, OUT1, OUT2, OUT3&lt;/LI&gt;&lt;LI&gt;Sample Rate: 48kHz&lt;/LI&gt;&lt;LI&gt;I2S format&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this is possible and do we have example code available?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Sep 2017 09:48:25 GMT</pubDate>
    <dc:creator>yuliucao</dc:creator>
    <dc:date>2017-09-12T09:48:25Z</dc:date>
    <item>
      <title>Simulate I2S on S32K144</title>
      <link>https://community.nxp.com/t5/S32K/Simulate-I2S-on-S32K144/m-p/700890#M1332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to setup a system which supports 2 channel input and 6 channel output on S32K144.&lt;/P&gt;&lt;P&gt;There was an example in SDK, but it only has 2 Channel input and 2 Channel output.&lt;/P&gt;&lt;P&gt;My system will look like:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;FlexIO pins configured as SCK, WS, IN1, OUT1, OUT2, OUT3&lt;/LI&gt;&lt;LI&gt;Sample Rate: 48kHz&lt;/LI&gt;&lt;LI&gt;I2S format&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this is possible and do we have example code available?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 09:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Simulate-I2S-on-S32K144/m-p/700890#M1332</guid>
      <dc:creator>yuliucao</dc:creator>
      <dc:date>2017-09-12T09:48:25Z</dc:date>
    </item>
  </channel>
</rss>