<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Problem in Receiving Message</title>
    <link>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388493#M13279</link>
    <description>&lt;P&gt;Hi, i am using s32k148 evaluation board and flashed a sample code of lpuart_echo example code. If i try to transmit and receive the data, the data is getting transmitted but we are not receiving any data.&lt;/P&gt;&lt;P&gt;Connections Made:&lt;/P&gt;&lt;P&gt;Using LPUART1&lt;/P&gt;&lt;P&gt;PTC6-RX connected to TX of TTL Converter&lt;/P&gt;&lt;P&gt;PTC7-TX connected to RX of TTL Converter&lt;/P&gt;&lt;P&gt;Evaluation Board Jumper Connections:&lt;/P&gt;&lt;P&gt;J22: 1,2&lt;/P&gt;&lt;P&gt;J7: 2,3&lt;/P&gt;&lt;P&gt;J8: 2,3&lt;/P&gt;&lt;P&gt;J18: 2,3&lt;/P&gt;&lt;P&gt;I have attached the snapshot of the Result that we are getting in DOCKLIGHT tool. If we send "Hello Board" message we are not receiving any reply back from the board. We are not receiving RX message&amp;nbsp; in the tool&lt;/P&gt;&lt;P&gt;Please let me know what connection we are missing and what is causing issue in Receiving the message. If any board connections are wrong or anything we are missing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Dec 2021 06:10:51 GMT</pubDate>
    <dc:creator>Arun07837</dc:creator>
    <dc:date>2021-12-17T06:10:51Z</dc:date>
    <item>
      <title>Problem in Receiving Message</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388493#M13279</link>
      <description>&lt;P&gt;Hi, i am using s32k148 evaluation board and flashed a sample code of lpuart_echo example code. If i try to transmit and receive the data, the data is getting transmitted but we are not receiving any data.&lt;/P&gt;&lt;P&gt;Connections Made:&lt;/P&gt;&lt;P&gt;Using LPUART1&lt;/P&gt;&lt;P&gt;PTC6-RX connected to TX of TTL Converter&lt;/P&gt;&lt;P&gt;PTC7-TX connected to RX of TTL Converter&lt;/P&gt;&lt;P&gt;Evaluation Board Jumper Connections:&lt;/P&gt;&lt;P&gt;J22: 1,2&lt;/P&gt;&lt;P&gt;J7: 2,3&lt;/P&gt;&lt;P&gt;J8: 2,3&lt;/P&gt;&lt;P&gt;J18: 2,3&lt;/P&gt;&lt;P&gt;I have attached the snapshot of the Result that we are getting in DOCKLIGHT tool. If we send "Hello Board" message we are not receiving any reply back from the board. We are not receiving RX message&amp;nbsp; in the tool&lt;/P&gt;&lt;P&gt;Please let me know what connection we are missing and what is causing issue in Receiving the message. If any board connections are wrong or anything we are missing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 06:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388493#M13279</guid>
      <dc:creator>Arun07837</dc:creator>
      <dc:date>2021-12-17T06:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in Receiving Message</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388565#M13281</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Arun07837" target="_blank" rel="noopener"&gt;Hi@Arun07837&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I checked your settings,these should be right.Did you set the baudrate wrong?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;For this example it is necessary to open a terminal emulator and configure it with:&lt;BR /&gt;- 115200 baud&lt;BR /&gt;- One stop bit&lt;BR /&gt;- No parity&lt;BR /&gt;- No flow control&lt;BR /&gt;- '\\n' line ending&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_1-1639721803840.png" style="width: 617px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165511i22BF363C83FC1A5E/image-dimensions/617x147?v=v2" width="617" height="147" role="button" title="Senlent_1-1639721803840.png" alt="Senlent_1-1639721803840.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_1-1639721803840.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; Jim,&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 06:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388565#M13281</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-12-17T06:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in Receiving Message</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388570#M13282</link>
      <description>&lt;P&gt;The settings are also correct, you can see the snapshot below&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Arun07837_0-1639722355677.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165512i7AEC9E46E1276071/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Arun07837_0-1639722355677.png" alt="Arun07837_0-1639722355677.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Arun07837_0-1639722355677.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 06:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388570#M13282</guid>
      <dc:creator>Arun07837</dc:creator>
      <dc:date>2021-12-17T06:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in Receiving Message</title>
      <link>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388577#M13283</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Arun07837" target="_blank"&gt;Hi@Arun07837&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please check if the correct port is selected.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1639722976543.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165513i232CEBF404FCFCE9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Senlent_0-1639722976543.png" alt="Senlent_0-1639722976543.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1639722976543.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can also use an oscilloscope to check the PTC6&amp;amp; PTC7.&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; Jim,&lt;/P&gt;</description>
      <pubDate>Fri, 17 Dec 2021 06:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-in-Receiving-Message/m-p/1388577#M13283</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-12-17T06:40:50Z</dc:date>
    </item>
  </channel>
</rss>