<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: AD conversion trigger</title>
    <link>https://community.nxp.com/t5/S32K/AD-conversion-trigger/m-p/1386306#M13228</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if the environment sensors have to be sampled at exact rate on both&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;ADC0 and ADC1 then you will need to use PDB to trigger both ADCs. Other sensors should be added to this which simplifies this a lot.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can refer to below example which shows possible implementation of multiple ADC conversions using SDK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope it helps.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Dec 2021 09:28:38 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2021-12-14T09:28:38Z</dc:date>
    <item>
      <title>AD conversion trigger</title>
      <link>https://community.nxp.com/t5/S32K/AD-conversion-trigger/m-p/1386113#M13220</link>
      <description>&lt;P&gt;I'm investigating how to efficiently perform multiple AD conversions.&lt;/P&gt;&lt;P&gt;There are environment sensors connected to ADC0 and ADC1, which is necessary to trigger the AD conversion at the same time with the exact cycle (e.g. every 10 ms) and transfer the AD value to memory via DMA.&lt;/P&gt;&lt;P&gt;In addition, different sensors for system diagnostics are also connected to ADC0 and ADC1, and need to read the AD value in the gap of the periodic AD conversion of the environment sensor.&lt;/P&gt;&lt;P&gt;If we need to read the two environment sensors at the correct cycle, how is it best to trigger it?&lt;/P&gt;&lt;P&gt;Also, what is the better trigger when reading the system diagnostic sensor in the gap between the readings of the environment sensor?&lt;/P&gt;&lt;P&gt;Please give me some advice on how to configure S32K.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 06:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AD-conversion-trigger/m-p/1386113#M13220</guid>
      <dc:creator>Hozumi</dc:creator>
      <dc:date>2021-12-14T06:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: AD conversion trigger</title>
      <link>https://community.nxp.com/t5/S32K/AD-conversion-trigger/m-p/1386306#M13228</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if the environment sensors have to be sampled at exact rate on both&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;ADC0 and ADC1 then you will need to use PDB to trigger both ADCs. Other sensors should be added to this which simplifies this a lot.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can refer to below example which shows possible implementation of multiple ADC conversions using SDK.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-PDB-ADC-DMA-S32DS-ARM-2018-R1/ta-p/1101686&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope it helps.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 09:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AD-conversion-trigger/m-p/1386306#M13228</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-12-14T09:28:38Z</dc:date>
    </item>
  </channel>
</rss>