<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to achieve Interrupt nesting  for S32K144 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386199#M13223</link>
    <description>&lt;P&gt;Now I use MCU S32K144, SDK version is 2.9.0.&lt;/P&gt;&lt;P&gt;I have used a DMA interrupt, lpit interrupt and CAN send/receive interrupt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the priority of all interrupt is the default value(0x00);&lt;/P&gt;&lt;P&gt;I wanted to DMA interrupt and lpit interrupt can interrupt CNA&amp;nbsp;CAN send/receive interrupt, So how to configure it? just configure the priority of&amp;nbsp;&amp;nbsp;DMA interrupt and lpit interrupt is less than the priority of&amp;nbsp;CNA&amp;nbsp;CAN send/receive interrupt?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Dec 2021 08:04:12 GMT</pubDate>
    <dc:creator>asd046012</dc:creator>
    <dc:date>2021-12-14T08:04:12Z</dc:date>
    <item>
      <title>How to achieve Interrupt nesting  for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386199#M13223</link>
      <description>&lt;P&gt;Now I use MCU S32K144, SDK version is 2.9.0.&lt;/P&gt;&lt;P&gt;I have used a DMA interrupt, lpit interrupt and CAN send/receive interrupt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the priority of all interrupt is the default value(0x00);&lt;/P&gt;&lt;P&gt;I wanted to DMA interrupt and lpit interrupt can interrupt CNA&amp;nbsp;CAN send/receive interrupt, So how to configure it? just configure the priority of&amp;nbsp;&amp;nbsp;DMA interrupt and lpit interrupt is less than the priority of&amp;nbsp;CNA&amp;nbsp;CAN send/receive interrupt?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 08:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386199#M13223</guid>
      <dc:creator>asd046012</dc:creator>
      <dc:date>2021-12-14T08:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to achieve Interrupt nesting  for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386342#M13230</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;There is also an system tick timer interrupt, I also hope that the DMA interrupt and the LPIT interrupt can interrupt the system tick interrupt.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; could this requirement&amp;nbsp; be achieved?&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 10:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386342#M13230</guid>
      <dc:creator>asd046012</dc:creator>
      <dc:date>2021-12-14T10:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to achieve Interrupt nesting  for S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386531#M13233</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/165390"&gt;@asd046012&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The DMA interrupt and the LPIT interrupt must have higher interrupt priorities than the SysTick and the FlexCAN.&lt;/P&gt;
&lt;P&gt;For example,&lt;/P&gt;
&lt;P&gt;DMA, LPIT: priority number 0 (default)&lt;/P&gt;
&lt;P&gt;FlexCAN, SysTick: priority number 1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The Systick priority is configurable in System Handler Priority Register 3, SHPR3.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;ARM®v7-M Architecture&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Reference Manual&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1639494675535.png" style="width: 705px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165147iCA0BB0FDB03F4FDF/image-dimensions/705x356?v=v2" width="705" height="356" role="button" title="danielmartynek_0-1639494675535.png" alt="danielmartynek_0-1639494675535.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="c"&gt;S32_SCB-&amp;gt;SHPR3 |= S32_SCB_SHPR3_PRI_15(0x10); // SysTick Priority 1&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 14 Dec 2021 15:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-achieve-Interrupt-nesting-for-S32K144/m-p/1386531#M13233</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-14T15:14:40Z</dc:date>
    </item>
  </channel>
</rss>