<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LIN specification in S32K</title>
    <link>https://community.nxp.com/t5/S32K/LIN-specification/m-p/1385551#M13207</link>
    <description>&lt;P&gt;Hi All,&amp;nbsp;&lt;/P&gt;&lt;P&gt;two questions:&lt;/P&gt;&lt;P&gt;NXP's LIN Stack supports specification v.2.2, V2.1, 1.3&amp;nbsp; and J2602 1.1.0.&lt;/P&gt;&lt;P&gt;- Are there any issues in using ldf files for v2.0?&lt;/P&gt;&lt;P&gt;- Is it possible to edit the lin stack for specification 2.0?&lt;/P&gt;&lt;P&gt;- Is there an implementation of NXP LIN stack for v2.0?&lt;/P&gt;&lt;P&gt;as a side note, we have following issue importing the ldf file:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Description Resource Path Location Type&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;(Error: line: 468 "FlashRequest"- Multi definitions for Diagnostic Master Request Schedule table.): Please change tab "LIN description file", change the file in "LDF file name" to Sources\Test.ldf for more inforfation (LDF file) can_pal_s32k146 lin_cfg/LDF file Processor Expert Problem&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Any hint on this topic?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;K.R.&lt;/P&gt;&lt;P&gt;L.T.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Dec 2021 09:43:47 GMT</pubDate>
    <dc:creator>luca_toso</dc:creator>
    <dc:date>2021-12-13T09:43:47Z</dc:date>
    <item>
      <title>LIN specification</title>
      <link>https://community.nxp.com/t5/S32K/LIN-specification/m-p/1385551#M13207</link>
      <description>&lt;P&gt;Hi All,&amp;nbsp;&lt;/P&gt;&lt;P&gt;two questions:&lt;/P&gt;&lt;P&gt;NXP's LIN Stack supports specification v.2.2, V2.1, 1.3&amp;nbsp; and J2602 1.1.0.&lt;/P&gt;&lt;P&gt;- Are there any issues in using ldf files for v2.0?&lt;/P&gt;&lt;P&gt;- Is it possible to edit the lin stack for specification 2.0?&lt;/P&gt;&lt;P&gt;- Is there an implementation of NXP LIN stack for v2.0?&lt;/P&gt;&lt;P&gt;as a side note, we have following issue importing the ldf file:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Description Resource Path Location Type&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;(Error: line: 468 "FlashRequest"- Multi definitions for Diagnostic Master Request Schedule table.): Please change tab "LIN description file", change the file in "LDF file name" to Sources\Test.ldf for more inforfation (LDF file) can_pal_s32k146 lin_cfg/LDF file Processor Expert Problem&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Any hint on this topic?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;K.R.&lt;/P&gt;&lt;P&gt;L.T.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 09:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-specification/m-p/1385551#M13207</guid>
      <dc:creator>luca_toso</dc:creator>
      <dc:date>2021-12-13T09:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: LIN specification</title>
      <link>https://community.nxp.com/t5/S32K/LIN-specification/m-p/1387324#M13257</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;please refer below answer from Stack SW team...&lt;/P&gt;
&lt;P&gt;- Are there any issues in using ldf files for v2.0?&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A] As far as I know, we can generate the configuration files normally.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;- Is it possible to edit the lin stack for specification 2.0?&lt;/P&gt;
&lt;P&gt;- Is there an implementation of NXP LIN stack for v2.0?&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A] Yes. The lin v2.0 is already supported from SDK K1 RTM 3.0.3 and above. Please check your SDK release version to make sure you are using the correct version.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;Description Resource Path Location Type&lt;BR /&gt;(Error: ....&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;[A]&lt;/FONT&gt; &lt;FONT color="#0000FF"&gt;It seems you have defined with multi Diagnostic Master request schedule table as below.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1639574235950.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165308i30629B70504187C2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1639574235950.jpeg" alt="PetrS_0-1639574235950.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_0-1639574235950.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;Currently, we do not support defined with multi diagnostic master request schedule table. So, please make sure we have only one schedule.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;I also share with you the ldf file example(Attached) which is supported the lin v2.0. You can refer it to more detail. (remove txt extension)&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_1-1639574235984.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/165309iF2C55E32A5EC7741/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_1-1639574235984.jpeg" alt="PetrS_1-1639574235984.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;PetrS_1-1639574235984.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 15 Dec 2021 13:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LIN-specification/m-p/1387324#M13257</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2021-12-15T13:20:40Z</dc:date>
    </item>
  </channel>
</rss>