<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using 2 SPI modules with a MUX for TPL loopback in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1382588#M13119</link>
    <description>&lt;P&gt;Hello Vishal,&lt;/P&gt;
&lt;P&gt;The MCU has 3 LPSPI instances + FlexIO that can emulate SPI.&lt;/P&gt;
&lt;P&gt;So why you don't use it?&lt;/P&gt;
&lt;P&gt;Anyway, we can't confirm that your proposed solution will work.&lt;/P&gt;
&lt;P&gt;This is really an application issue.&lt;/P&gt;
&lt;P&gt;If you have any specific questions on the LPSPI / FlexIO WH, please let me know,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Dec 2021 10:31:25 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2021-12-07T10:31:25Z</dc:date>
    <item>
      <title>Using 2 SPI modules with a MUX for TPL loopback</title>
      <link>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1381897#M13095</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;At any point of time only&amp;nbsp; one TPL Transceiver is active on the bus i.e., Half duplex. So can we use 2 SPI's instead of 3 as we have Enable options for 2 transceivers as shown in the figure below ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SPI1 used as Master and SPI2 is used as Slave" style="width: 531px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164186i4EC8A4D903C536A3/image-size/large?v=v2&amp;amp;px=999" role="button" title="loopback_using_2SPI.drawio.png" alt="SPI1 used as Master and SPI2 is used as Slave" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;SPI1 used as Master and SPI2 is used as Slave&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;R!&lt;/P&gt;&lt;P&gt;Vishal&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 10:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1381897#M13095</guid>
      <dc:creator>Vishal_Pandey</dc:creator>
      <dc:date>2021-12-06T10:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: Using 2 SPI modules with a MUX for TPL loopback</title>
      <link>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1382588#M13119</link>
      <description>&lt;P&gt;Hello Vishal,&lt;/P&gt;
&lt;P&gt;The MCU has 3 LPSPI instances + FlexIO that can emulate SPI.&lt;/P&gt;
&lt;P&gt;So why you don't use it?&lt;/P&gt;
&lt;P&gt;Anyway, we can't confirm that your proposed solution will work.&lt;/P&gt;
&lt;P&gt;This is really an application issue.&lt;/P&gt;
&lt;P&gt;If you have any specific questions on the LPSPI / FlexIO WH, please let me know,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 10:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1382588#M13119</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-07T10:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: Using 2 SPI modules with a MUX for TPL loopback</title>
      <link>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1382810#M13127</link>
      <description>&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;Thanks for responding ! Flex IO is being used for an other application peripheral(memory). It will be helpful if&amp;nbsp; you can point out the drawbacks of using 2 SPI modules then I&amp;nbsp; can think of emulating SPI through External IC or USART.&amp;nbsp;&lt;/P&gt;&lt;P&gt;R ,&lt;/P&gt;&lt;P&gt;Vishal&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 17:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1382810#M13127</guid>
      <dc:creator>Vishal_Pandey</dc:creator>
      <dc:date>2021-12-07T17:43:04Z</dc:date>
    </item>
    <item>
      <title>Re: Using 2 SPI modules with a MUX for TPL loopback</title>
      <link>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1383998#M13168</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194183"&gt;@Vishal_Pandey&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It is difficult for me to review the design because I don't know the use case.&lt;/P&gt;
&lt;P&gt;If the two transceivers don't start transfers at the same it, it should be feasible.&lt;/P&gt;
&lt;P&gt;As I said, it is an application issue.&lt;/P&gt;
&lt;P&gt;If you have any questions on the LPSPI, FlexIO modules or the MCU overall, please let me know,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Dec 2021 11:13:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-2-SPI-modules-with-a-MUX-for-TPL-loopback/m-p/1383998#M13168</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-09T11:13:59Z</dc:date>
    </item>
  </channel>
</rss>