<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPIO toggle delay in S32K</title>
    <link>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1381978#M13100</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have programmed S32K144 to make a gpio pin high on main function and also configured it as pull down on processor expert. The problem is, after giving the controller 5v supply it was taking 16 milliseconds to make this pin high. How can I reduce this 16ms delay as minimum as possible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Prashanth Reddy&lt;/P&gt;</description>
    <pubDate>Mon, 06 Dec 2021 12:58:02 GMT</pubDate>
    <dc:creator>preddy</dc:creator>
    <dc:date>2021-12-06T12:58:02Z</dc:date>
    <item>
      <title>GPIO toggle delay</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1381978#M13100</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have programmed S32K144 to make a gpio pin high on main function and also configured it as pull down on processor expert. The problem is, after giving the controller 5v supply it was taking 16 milliseconds to make this pin high. How can I reduce this 16ms delay as minimum as possible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Prashanth Reddy&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 12:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1381978#M13100</guid>
      <dc:creator>preddy</dc:creator>
      <dc:date>2021-12-06T12:58:02Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO toggle delay</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1382057#M13104</link>
      <description>&lt;P&gt;Hi Preddy ,&lt;/P&gt;&lt;P&gt;it's a pleasure to talk with you. i have some method&amp;nbsp; for you reference.&lt;/P&gt;&lt;P&gt;1)write code in machine/assembly language.&lt;/P&gt;&lt;P&gt;2)review the capability of the hardware , the GPIO's responds need some time, the PCB layout wire also need to reduce the stray capacitance if you don't have measure the GPIO pin directly.&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;Guofred&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 15:40:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1382057#M13104</guid>
      <dc:creator>Guofred</dc:creator>
      <dc:date>2021-12-06T15:40:06Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO toggle delay</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1382250#M13105</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check if the answers in the post are helpful:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/watchdog-driver-initialize-of-SDK-cost-too-much-time/td-p/1206555" target="_self"&gt;watchdog driver initialize of SDK cost too much time&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 01:24:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-toggle-delay/m-p/1382250#M13105</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-12-07T01:24:15Z</dc:date>
    </item>
  </channel>
</rss>