<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPIO PWM low voltage not at ground in S32K</title>
    <link>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699443#M1308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is due to the LED.&lt;/P&gt;&lt;P&gt;Reroute the PWM channel to another pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Aug 2017 13:59:00 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-08-17T13:59:00Z</dc:date>
    <item>
      <title>GPIO PWM low voltage not at ground</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699442#M1307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using PWM to drive a circuit off of PTD16 and am observing a low voltage of 440mV, instead of 0V (GND) as I might expect. &amp;nbsp;The high voltage is 5V. &amp;nbsp;This happens for 0% through 100% duty cycle.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using pin PTD16 (connected to the GREEN_LED feature on the S32K144 development board). &amp;nbsp;It doesn't seem to matter if I put a pull down resistor (internal or external) in place. &amp;nbsp;There is no documentation on what the GPIO low voltage out should be. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this known behavior? &amp;nbsp;If so is there a way to reference to GND instead of 440mV? &amp;nbsp;Does it depend on which pin or drive strength is being used? My application needs PWM that can go from 0V to 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best,&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 13:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699442#M1307</guid>
      <dc:creator>fredericksoo</dc:creator>
      <dc:date>2017-08-16T13:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO PWM low voltage not at ground</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699443#M1308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is due to the LED.&lt;/P&gt;&lt;P&gt;Reroute the PWM channel to another pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 13:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699443#M1308</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-08-17T13:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO PWM low voltage not at ground</title>
      <link>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699444#M1309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that worked. &amp;nbsp;Forgot that when pulling low, LED is still connected and causing current to flow. &amp;nbsp;The circuit is Vdd-&amp;gt;LED-&amp;gt;current-limiting resistor (Rc)-&amp;gt;pin-&amp;gt;R-&amp;gt;GND so a voltage divider is formed between Rc and R. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With LED forward voltage of ~3V, Rc&amp;nbsp;of 220ohms and Vdd = 5V, if I see 440mV at my measurement point, R ~ 64ohms. &amp;nbsp;This is close to what I actually measure. &amp;nbsp;Will use this as the value in my circuit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 15:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GPIO-PWM-low-voltage-not-at-ground/m-p/699444#M1309</guid>
      <dc:creator>fredericksoo</dc:creator>
      <dc:date>2017-08-17T15:41:18Z</dc:date>
    </item>
  </channel>
</rss>