<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K3 Read/Write Flash with C40-Driver</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1380459#M13058</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to read and write some data to the internal flash of the S32K344. I use the C40 Dreiver for this and the example from the S32DS. If I do delete -&amp;gt; write -&amp;gt; read once, it works fine and I can see the change immediately in the memory browser. But the second time it seems to have no effect in flash memory. If I restart the code with the debugger, I can see the changed data in flash from the second write.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What else needs to be taken care of so that each erase-&amp;gt;write operation immediately writes the data to flash memory?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JoDo&lt;/P&gt;</description>
    <pubDate>Thu, 02 Dec 2021 08:33:45 GMT</pubDate>
    <dc:creator>JoDo</dc:creator>
    <dc:date>2021-12-02T08:33:45Z</dc:date>
    <item>
      <title>S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1380459#M13058</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to read and write some data to the internal flash of the S32K344. I use the C40 Dreiver for this and the example from the S32DS. If I do delete -&amp;gt; write -&amp;gt; read once, it works fine and I can see the change immediately in the memory browser. But the second time it seems to have no effect in flash memory. If I restart the code with the debugger, I can see the changed data in flash from the second write.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What else needs to be taken care of so that each erase-&amp;gt;write operation immediately writes the data to flash memory?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JoDo&lt;/P&gt;</description>
      <pubDate>Thu, 02 Dec 2021 08:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1380459#M13058</guid>
      <dc:creator>JoDo</dc:creator>
      <dc:date>2021-12-02T08:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1381996#M13102</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191027"&gt;@JoDo&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I had to copy your code to C40_Ip_Example_S32K344 from RTD 1.0.0 2010_10 version as I don't have the older version that you use.&lt;/P&gt;
&lt;P&gt;Anyway, without any modification, I can see the data in the memory after the second write.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1638797191542.png" style="width: 763px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164209i93DC6DC2A8592A27/image-dimensions/763x611?v=v2" width="763" height="611" role="button" title="danielmartynek_0-1638797191542.png" alt="danielmartynek_0-1638797191542.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What debugger do you use?&lt;/P&gt;
&lt;P&gt;Can you update to the new RTD?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 13:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1381996#M13102</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-06T13:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1382046#M13103</link>
      <description>&lt;P&gt;thanks for sharing this information. it looks the flash had been written successful in the second time after restarting the code with the debugger, i also think due to the software version or debugger setting cause this issue.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 15:15:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1382046#M13103</guid>
      <dc:creator>Guofred</dc:creator>
      <dc:date>2021-12-06T15:15:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1382596#M13120</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194014"&gt;@Guofred&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Since I can't reproduce it, I'm not sure I full understand the issue.&lt;/P&gt;
&lt;P&gt;You read the flash with core and the debugger.&lt;/P&gt;
&lt;P&gt;Do they both show the same issue, or is it just the debugger (memory view)?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 10:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1382596#M13120</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-07T10:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1383430#M13144</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194014"&gt;@Guofred&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you very much for the answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I checked the code with the new RTD version and the flash could be read and written several times. It seems that the problem was indeed in the old RTD version.&lt;/P&gt;&lt;P&gt;The strange thing was that I could write several times and could also read the data in memory, but it stopped working once I ran the read function.&lt;/P&gt;&lt;P&gt;However, with the new RTD version everything works fine.&lt;BR /&gt;Tank you for the advice!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;JoDo&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 12:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1383430#M13144</guid>
      <dc:creator>JoDo</dc:creator>
      <dc:date>2021-12-08T12:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1383435#M13146</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191027"&gt;@JoDo&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for the update,&lt;/P&gt;
&lt;P&gt;I'm glad it works now,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 13:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1383435#M13146</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-12-08T13:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Read/Write Flash with C40-Driver</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1493217#M16550</link>
      <description>&lt;P&gt;what is c40? Is it standard or what?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 09:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Read-Write-Flash-with-C40-Driver/m-p/1493217#M16550</guid>
      <dc:creator>Skannan</dc:creator>
      <dc:date>2022-07-21T09:23:50Z</dc:date>
    </item>
  </channel>
</rss>