<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RESET_B pin manual control in S32K</title>
    <link>https://community.nxp.com/t5/S32K/RESET-B-pin-manual-control/m-p/1375697#M12887</link>
    <description>&lt;P&gt;Hi, i am using s32k118 and i was wondering if its possible to use the reset_b pin as an output, as i want to control the reset_b pin order to put it low whenever i want.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Nov 2021 14:07:03 GMT</pubDate>
    <dc:creator>riglesias2021</dc:creator>
    <dc:date>2021-11-23T14:07:03Z</dc:date>
    <item>
      <title>RESET_B pin manual control</title>
      <link>https://community.nxp.com/t5/S32K/RESET-B-pin-manual-control/m-p/1375697#M12887</link>
      <description>&lt;P&gt;Hi, i am using s32k118 and i was wondering if its possible to use the reset_b pin as an output, as i want to control the reset_b pin order to put it low whenever i want.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Nov 2021 14:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RESET-B-pin-manual-control/m-p/1375697#M12887</guid>
      <dc:creator>riglesias2021</dc:creator>
      <dc:date>2021-11-23T14:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: RESET_B pin manual control</title>
      <link>https://community.nxp.com/t5/S32K/RESET-B-pin-manual-control/m-p/1376604#M12910</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;FTFC_FOPT&lt;/STRONG&gt;[&lt;STRONG&gt;RESET_PIN_CFG&lt;/STRONG&gt;] can be used to disable the RESET_b function. But: there could be a short period of contention during a POR ramp where the MCU drives the pin low prior to establishing the setting of this option and releasing the reset function on the pin.&lt;BR /&gt;It is not recommended to use the RESET_b pin as a normal IO port.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FTFC_FOPT[RESET_PIN_CFG].png" style="width: 928px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/163135iA4B221057DE2F858/image-size/large?v=v2&amp;amp;px=999" role="button" title="FTFC_FOPT[RESET_PIN_CFG].png" alt="FTFC_FOPT[RESET_PIN_CFG].png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 25 Nov 2021 00:41:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RESET-B-pin-manual-control/m-p/1376604#M12910</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2021-11-25T00:41:59Z</dc:date>
    </item>
  </channel>
</rss>