<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need sample code for CAN and PWM in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Need-sample-code-for-CAN-and-PWM/m-p/1372214#M12814</link>
    <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;Could you please share below sample code for S32k144 series MCUS,&lt;/P&gt;&lt;P&gt;1. Can communication&lt;/P&gt;&lt;P&gt;2.PWM&lt;/P&gt;&lt;P&gt;is there any sample code for CAN signal to PWM signal conversion, if so then pls share that code also.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pratyay&lt;/P&gt;</description>
    <pubDate>Tue, 16 Nov 2021 21:31:42 GMT</pubDate>
    <dc:creator>pratayay123</dc:creator>
    <dc:date>2021-11-16T21:31:42Z</dc:date>
    <item>
      <title>Need sample code for CAN and PWM</title>
      <link>https://community.nxp.com/t5/S32K/Need-sample-code-for-CAN-and-PWM/m-p/1372214#M12814</link>
      <description>&lt;P&gt;Dear Team,&lt;/P&gt;&lt;P&gt;Could you please share below sample code for S32k144 series MCUS,&lt;/P&gt;&lt;P&gt;1. Can communication&lt;/P&gt;&lt;P&gt;2.PWM&lt;/P&gt;&lt;P&gt;is there any sample code for CAN signal to PWM signal conversion, if so then pls share that code also.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pratyay&lt;/P&gt;</description>
      <pubDate>Tue, 16 Nov 2021 21:31:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-sample-code-for-CAN-and-PWM/m-p/1372214#M12814</guid>
      <dc:creator>pratayay123</dc:creator>
      <dc:date>2021-11-16T21:31:42Z</dc:date>
    </item>
    <item>
      <title>Re: Need sample code for CAN and PWM</title>
      <link>https://community.nxp.com/t5/S32K/Need-sample-code-for-CAN-and-PWM/m-p/1372351#M12819</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@pratayay123" target="_blank" rel="noopener"&gt;Hi@pratayay123&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1.About CAN communication you can refer to example:'&lt;FONT color="#0000FF"&gt;&lt;STRONG&gt;flexcan_enerypted_s32k144&lt;/STRONG&gt;&lt;/FONT&gt;' or "&lt;FONT color="#0000FF"&gt;&lt;STRONG&gt;can_pal_s32k144&lt;/STRONG&gt;&lt;/FONT&gt;",those two examples will show the usage of the FlexCAN module.&lt;/P&gt;
&lt;P&gt;2.About PWM ,you can refer to example:"&lt;FONT color="#0000FF"&gt;&lt;STRONG&gt;ftm_pwm_s32k144&lt;/STRONG&gt;&lt;/FONT&gt;",this example using a single channel to light a LED on the S32K144EVB board.The light's intensity is increased and decreased periodically.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Above example code can be found in SDK: &lt;STRONG&gt;S32K1xx RTM 3.0.0&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;And there is no such sample code for CAN signal related to PWM signal conversion ,so you need to write the application program by youself.&lt;/P&gt;
&lt;P&gt;BR!&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Jim,&lt;/P&gt;
&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 03:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-sample-code-for-CAN-and-PWM/m-p/1372351#M12819</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2021-11-17T03:25:31Z</dc:date>
    </item>
  </channel>
</rss>