<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32DS example Project S32K144_CAN_MASTER_Example can‘t work in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695455#M1269</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use FRDM-s32k144 board to &amp;nbsp;test flexcan. I deleted the code about sbc because the board uses tja1050 instead of sbc. When I ran this &amp;nbsp;project, it was jammed at &amp;nbsp;"while(FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, RX_MAILBOX) == STATUS_BUSY);" and&amp;nbsp;TXERRCNT of ECR is 0x80, I get a "Error&amp;nbsp;Passive" state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the clocks and gpio,but found nothing wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Aug 2017 03:50:49 GMT</pubDate>
    <dc:creator>aliaszhang</dc:creator>
    <dc:date>2017-08-10T03:50:49Z</dc:date>
    <item>
      <title>S32DS example Project S32K144_CAN_MASTER_Example can‘t work</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695455#M1269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use FRDM-s32k144 board to &amp;nbsp;test flexcan. I deleted the code about sbc because the board uses tja1050 instead of sbc. When I ran this &amp;nbsp;project, it was jammed at &amp;nbsp;"while(FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, RX_MAILBOX) == STATUS_BUSY);" and&amp;nbsp;TXERRCNT of ECR is 0x80, I get a "Error&amp;nbsp;Passive" state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the clocks and gpio,but found nothing wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 03:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695455#M1269</guid>
      <dc:creator>aliaszhang</dc:creator>
      <dc:date>2017-08-10T03:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS example Project S32K144_CAN_MASTER_Example can‘t work</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695456#M1270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the transceiver is not connected to the bus with other nodes, this behavior is normal.&lt;/P&gt;&lt;P&gt;The FlexCAN is sending a message, but it is not ACKed from other node(s), the MB flag is not set, &amp;nbsp;message is transmitted again and again and FlexCAN module stays in Error passive state with ECR=0x80.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need to connect other board with CAN_SLAVE_example to make this running.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; You can also enable “Loopback” mode in the Component inspector and test TX/RX operation on single board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 07:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695456#M1270</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-08-10T07:53:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS example Project S32K144_CAN_MASTER_Example can‘t work</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695457#M1271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,Petr&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, I connected two board together to achive this function. One work as a "master",and another work as "slave".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both boards use the can0, and &amp;nbsp;the connection is GND to GND, CL0 to CL0, CH0 to CH0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am trying to make sure that the chip Tja1050 is working .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;xiong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Aug 2017 08:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-example-Project-S32K144-CAN-MASTER-Example-can-t-work/m-p/695457#M1271</guid>
      <dc:creator>aliaszhang</dc:creator>
      <dc:date>2017-08-11T08:56:01Z</dc:date>
    </item>
  </channel>
</rss>