<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FlexRAM loading timing at Reset in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FlexRAM-loading-timing-at-Reset/m-p/693714#M1241</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Per application note AN11983, it was highlighted the ability to select if RESET signal is to be released before or &lt;BR /&gt;after FlexRAM loading from FlexNVM is completed or not during reset, via the FCCOB3 for the "Program Partition"&lt;BR /&gt; command, i.e.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10322i31477915C4CE9FAC/image-size/large?v=v2&amp;amp;px=999" title="Table 33-37 (RM) - Program Partition Command.gif" alt="Table 33-37 (RM) - Program Partition Command.gif" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Is there a specification, or an estimate on the time taken for the FlexRAM to be loaded (i.e. before EEERDY gets set)&lt;BR /&gt;during these boot/reset process, i.e.&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10372i41EF52793EABF49E/image-size/large?v=v2&amp;amp;px=999" title="Figure 5 (AN11983) - FlexRAM loading timing.gif" alt="Figure 5 (AN11983) - FlexRAM loading timing.gif" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;I believe timing may depend on some factors, clearly the EE/FlexRAM size used, but are there any other factors&lt;BR /&gt;this will depend on? Since this has direct implication on boot timing, and whether to allow CPU to perform other &lt;BR /&gt;tasks while FlexRAM is updated, or wait for FlexRAM to be fully loaded first, i.e. the absolutely safe approach.&lt;BR /&gt;&lt;BR /&gt;Also, is the algorithm of the internal EEPROM emulation state machine something that is available for review?&amp;nbsp; &lt;BR /&gt;If so, then the information above could be understood better as well.&lt;BR /&gt;&lt;BR /&gt;Thanks for any help with the above.&lt;BR /&gt;N.H.Ching&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Aug 2017 08:55:35 GMT</pubDate>
    <dc:creator>N_H_</dc:creator>
    <dc:date>2017-08-04T08:55:35Z</dc:date>
    <item>
      <title>FlexRAM loading timing at Reset</title>
      <link>https://community.nxp.com/t5/S32K/FlexRAM-loading-timing-at-Reset/m-p/693714#M1241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Per application note AN11983, it was highlighted the ability to select if RESET signal is to be released before or &lt;BR /&gt;after FlexRAM loading from FlexNVM is completed or not during reset, via the FCCOB3 for the "Program Partition"&lt;BR /&gt; command, i.e.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10322i31477915C4CE9FAC/image-size/large?v=v2&amp;amp;px=999" title="Table 33-37 (RM) - Program Partition Command.gif" alt="Table 33-37 (RM) - Program Partition Command.gif" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Is there a specification, or an estimate on the time taken for the FlexRAM to be loaded (i.e. before EEERDY gets set)&lt;BR /&gt;during these boot/reset process, i.e.&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/10372i41EF52793EABF49E/image-size/large?v=v2&amp;amp;px=999" title="Figure 5 (AN11983) - FlexRAM loading timing.gif" alt="Figure 5 (AN11983) - FlexRAM loading timing.gif" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;I believe timing may depend on some factors, clearly the EE/FlexRAM size used, but are there any other factors&lt;BR /&gt;this will depend on? Since this has direct implication on boot timing, and whether to allow CPU to perform other &lt;BR /&gt;tasks while FlexRAM is updated, or wait for FlexRAM to be fully loaded first, i.e. the absolutely safe approach.&lt;BR /&gt;&lt;BR /&gt;Also, is the algorithm of the internal EEPROM emulation state machine something that is available for review?&amp;nbsp; &lt;BR /&gt;If so, then the information above could be understood better as well.&lt;BR /&gt;&lt;BR /&gt;Thanks for any help with the above.&lt;BR /&gt;N.H.Ching&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 08:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexRAM-loading-timing-at-Reset/m-p/693714#M1241</guid>
      <dc:creator>N_H_</dc:creator>
      <dc:date>2017-08-04T08:55:35Z</dc:date>
    </item>
  </channel>
</rss>