<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: GptChannelClkSrcRef - where is it in the code</title>
    <link>https://community.nxp.com/t5/S32K/GptChannelClkSrcRef-where-is-it-in-the-code/m-p/1353191#M12396</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191531"&gt;@Kanaqw&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If user change the&amp;nbsp;&lt;SPAN&gt;GptChannelClkSrcRef, the value GptChannelTickFrequency will also need to change/update. And it will show to the tick frequency of the timer in the bus with this GPT channel clock(Note that user need to choose the correct reference clock which they have set up by the MCU module). And yes, the GptChannelClkSrcRef will not effect the generated configuration of the GPT channel(but if user choose the wrong reference clock, the real frequency of the GPT channel will be not the same with the GptChannelTickFrequency). But it will effect another module which use this GPT channel (Eg WDG).&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Hung&lt;/P&gt;</description>
    <pubDate>Mon, 11 Oct 2021 03:08:28 GMT</pubDate>
    <dc:creator>hungnguyenphi</dc:creator>
    <dc:date>2021-10-11T03:08:28Z</dc:date>
    <item>
      <title>GptChannelClkSrcRef - where is it in the code</title>
      <link>https://community.nxp.com/t5/S32K/GptChannelClkSrcRef-where-is-it-in-the-code/m-p/1351951#M12370</link>
      <description>&lt;P&gt;Here's the question. I'm changing config files in tresos, e.g.&amp;nbsp;GptChannelClkSrcRef, but after I generate config, code doesnt change. Gpt_Cfg.c, Gpt_Cfg.h, Gpt_PBcfg.c - all same. Maybe I dont understand something? Code doesnt have errors. Maybe it is in another module (but not in mcu, I've checked that already)&lt;/P&gt;</description>
      <pubDate>Thu, 07 Oct 2021 14:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GptChannelClkSrcRef-where-is-it-in-the-code/m-p/1351951#M12370</guid>
      <dc:creator>Kanaqw</dc:creator>
      <dc:date>2021-10-07T14:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: GptChannelClkSrcRef - where is it in the code</title>
      <link>https://community.nxp.com/t5/S32K/GptChannelClkSrcRef-where-is-it-in-the-code/m-p/1353191#M12396</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191531"&gt;@Kanaqw&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If user change the&amp;nbsp;&lt;SPAN&gt;GptChannelClkSrcRef, the value GptChannelTickFrequency will also need to change/update. And it will show to the tick frequency of the timer in the bus with this GPT channel clock(Note that user need to choose the correct reference clock which they have set up by the MCU module). And yes, the GptChannelClkSrcRef will not effect the generated configuration of the GPT channel(but if user choose the wrong reference clock, the real frequency of the GPT channel will be not the same with the GptChannelTickFrequency). But it will effect another module which use this GPT channel (Eg WDG).&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Hung&lt;/P&gt;</description>
      <pubDate>Mon, 11 Oct 2021 03:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/GptChannelClkSrcRef-where-is-it-in-the-code/m-p/1353191#M12396</guid>
      <dc:creator>hungnguyenphi</dc:creator>
      <dc:date>2021-10-11T03:08:28Z</dc:date>
    </item>
  </channel>
</rss>