<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K148 Secure Boot</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-Secure-Boot/m-p/1350917#M12343</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question for S32K secure boot:&lt;/P&gt;&lt;P&gt;We are using mac generation and verification mechanism from CSEc for secure boot functionality.&lt;/P&gt;&lt;P&gt;As mentioned in below snap from S32K manual, We can use maximum size of data limited to be no more than one read partition,&lt;/P&gt;&lt;P&gt;or less if the starting address is not the start of the read partition.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wanglijun_0-1633501400449.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158337i02D2E2B861D28CCB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wanglijun_0-1633501400449.jpeg" alt="wanglijun_0-1633501400449.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;wanglijun_0-1633501400449.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In our case we are using S32k148, so maximum CMAC can be calculated on 512KB program flash block.&lt;/P&gt;&lt;P&gt;For our project, application area is from 0x50000 – 0x11FFFF which is located on multiple read partitions.&lt;/P&gt;&lt;P&gt;I this case we are facing the issue of cmac calculation over application area.&lt;/P&gt;&lt;P&gt;Can you please support to find out the solution for mac generation over above mentioned application area?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Wang Lijun&lt;/P&gt;</description>
    <pubDate>Wed, 06 Oct 2021 06:23:42 GMT</pubDate>
    <dc:creator>wanglijun</dc:creator>
    <dc:date>2021-10-06T06:23:42Z</dc:date>
    <item>
      <title>S32K148 Secure Boot</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-Secure-Boot/m-p/1350917#M12343</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a question for S32K secure boot:&lt;/P&gt;&lt;P&gt;We are using mac generation and verification mechanism from CSEc for secure boot functionality.&lt;/P&gt;&lt;P&gt;As mentioned in below snap from S32K manual, We can use maximum size of data limited to be no more than one read partition,&lt;/P&gt;&lt;P&gt;or less if the starting address is not the start of the read partition.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wanglijun_0-1633501400449.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158337i02D2E2B861D28CCB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wanglijun_0-1633501400449.jpeg" alt="wanglijun_0-1633501400449.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;wanglijun_0-1633501400449.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In our case we are using S32k148, so maximum CMAC can be calculated on 512KB program flash block.&lt;/P&gt;&lt;P&gt;For our project, application area is from 0x50000 – 0x11FFFF which is located on multiple read partitions.&lt;/P&gt;&lt;P&gt;I this case we are facing the issue of cmac calculation over application area.&lt;/P&gt;&lt;P&gt;Can you please support to find out the solution for mac generation over above mentioned application area?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Wang Lijun&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 06:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-Secure-Boot/m-p/1350917#M12343</guid>
      <dc:creator>wanglijun</dc:creator>
      <dc:date>2021-10-06T06:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 Secure Boot</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-Secure-Boot/m-p/1351088#M12348</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I just answered the same question here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Handling-of-CMAC-operations-for-application-spread-over-two-read/m-p/1350904/highlight/false#M12342" target="_blank"&gt;https://community.nxp.com/t5/S32K/Handling-of-CMAC-operations-for-application-spread-over-two-read/m-p/1350904/highlight/false#M12342&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 06 Oct 2021 11:18:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-Secure-Boot/m-p/1351088#M12348</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-10-06T11:18:02Z</dc:date>
    </item>
  </channel>
</rss>